This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 16-bit SPI/EDMA transfers via PSP - alterations from 8-bit transfer

Hi Again

Still have no replies to this post

http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/168604.aspx#615313

Has anyone tried or had issues getting 16-bit SPI transfers to work with DSP as master interfacing to a FPGA. Our 8-bit transfers work without issue though can't understand why the 16-bit transfers only increment addresses by a byte each time (described with pretty pictures hey..hey.. in the above link)?

Or perhaps the question to ask is

What is required to convert a 8-bit SPI/EDMA3 transfer to a 16-bit SPI/EDMA3 transfer (we are using the GIO_submit() invocation) ?

Can post additional details as needed...

Many Thanks

Barry