This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127 IPNC Boot message problem



Hi all

 

Target H/W : DM8127 IPNC

Software Version : 2.0.0

 

After download new software version 2.0.0, there is no console message but HDMI out and PC side streaming is OK.

Below is the boot logo until boot message is OK

 

U-Boot 2010.06 (Mar 07 2012 - 17:30:47) DM812x_IPNC_2.00.00

TI8148-GP rev 2.1

ARM clk: 600MHz
DDR clk: 400MHz
IVA clk: 450MHz
ISS clk: 400MHz
DSP clk: 400MHz
DSS clk: 200MHz

DRAM:  512 MiB
NAND:  HW ECC Hamming Code selected
256 MiB
Using default environment

The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
Hit any key to stop autoboot:  0

NAND read: device 0 offset 0x20000, size 0x40000
 262144 bytes read: OK
## Starting application at 0x81000000 ...

U-Boot 2010.06 (Mar 07 2012 - 17:31:21) DM812x_IPNC_2.00.00

TI8148-GP rev 2.1

ARM clk: 600MHz
DDR clk: 400MHz
IVA clk: 450MHz
ISS clk: 400MHz
DSP clk: 400MHz
DSS clk: 200MHz

I2C:   ready
DRAM:  512 MiB
NAND:  HW ECC Hamming Code selected
256 MiB
MMC:   OMAP SD/MMC: 0, ON-BOARD SDIO: 1
                          .:;rrr;;.
                    ,5#@@@@#####@@@@@@#2,
                 ,A@@@hi;;;r5;;;;r;rrSG@@@A,
               r@@#i;:;s222hG;rrsrrrrrr;ri#@@r
             :@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@:
            B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B
           @@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@
          @@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@
         @@;;rrsrrs@MB#@@@@@###@@@@@@#rsrsrsrsrr;;@@
        G@r;rrsrsr;#X;SX25Ss#@@#M@#9H9rrsrsrsrsrs;r@G
        @9:srsrsrs;2@;:;;:.X@@@@@H::;rrsrsrsrsrsrr:3@
       X@;rrsrsrsrr;XAi;;:&@@#@Bs:rrsrsrsrsrsrsrsrr;@X
       @#;rsrsrsrsrr;r2ir@@@###::rrsrsrsrsrsrsrsrsr:@@
       @A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@
       @&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@
       @#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@
       M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@#
       :@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@,
        @@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@
         @A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@
         ;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@;
          r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r
           ,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@,
             B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H
              .@@@i;;rrrrsrs2i;rrrrr;r@M:;i@@@.
                .A@@#5r;;;r;;;rrr;r:r#AsM@@H.
                   ;&@@@@MhXS5i5SX9B@@@@G;
                       :ihM#@@@@@##hs,

Date: 2011-03-17 (Thursday)    Time: 11:35:36
Net:   Detected MACID:0:c:c:a0:8:83
cpsw
Hit any key to stop autoboot:  0
link up on port 0, speed 1000, full duplex
Using cpsw device
TFTP from server 192.168.10.94; our IP address is 192.168.10.194
Filename 'uImage'.
Load address: 0x81000000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ####################################################
done
Bytes transferred = 2262792 (228708 hex)
## Booting kernel from Legacy Image at 81000000 ...
   Image Name:   Linux-2.6.37_DM812x_IPNC_2.00.00
   Created:      2012-02-14   8:21:36 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2262728 Bytes = 2.2 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37_DM812x_IPNC_2.00.00 (a0875405@bangvideoapps01) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 PREEMPT Tue Feb 14 13:51:32 IST 2012
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8148ipnc
vram size = 4194304 at 0x0
bootconsole [earlycon0] enabled
reserved size = 4194304 at 0x0
FB: Reserving 4194304 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8148 2.0
SRAM: Mapped pa 0x40300000 to va 0xfe400000 size: 0x20000
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 19296
Kernel command line: console=tty00,115200n8 root=/dev/nfs rw mem=80M vram=4M notifyk.vpssm3_sva=0xBFD00000 nfsroot=192.168.10.94:/home/pine/dm8127/IPNetCam/ipnc_rdk/target/filesys,nolock eth=$(ethaddr) ip=dhcp earlyprintk
cpsw: kernel boot params Ethernet address: $(ethaddr)
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 76MB = 76MB total
Memory: 72132k/72132k available, 9788k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xffc00000 - 0xffe00000   (   2 MB)
    vmalloc : 0xc5800000 - 0xf8000000   ( 808 MB)
    lowmem  : 0xc0000000 - 0xc5000000   (  80 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .init : 0xc0008000 - 0xc0036000   ( 184 kB)
      .text : 0xc0036000 - 0xc0455000   (4220 kB)
      .data : 0xc0456000 - 0xc0491ec0   ( 240 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:375
omap_hwmod: gpio4: softreset failed (waited 10000 usec)
IRQ: Found an INTCat 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ368
Trying to install interrupt handler for IRQ369
Trying to install interrupt handler for IRQ370
Trying to install interrupt handler for IRQ371
Trying to install interrupt handler for IRQ372
Trying to install interrupt handler for IRQ373
Trying to install interrupt handler for IRQ374
Trying to install type control for IRQ375
Trying to set irq flags for IRQ375
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
console [tty0] enabled, bootconsole disabled

 

Thanks in advance.

Hennessy

 

 

 

  • Hi all

     

    This is my mistake at boot argument.

     

    Original argument :

    setenv bootargs 'mem=80M vram=4M notifyk.vpssm3_sva=0xBFD00000 console=tty00,115200n8 noinitrd root=/dev/mtdblock4  rw rootfstype=jffs2 ip=dhcp eth=$(ethaddr) earlyprintk'

     

    Fixed argument :

    setenv bootargs 'mem=80M vram=4M notifyk.vpssm3_sva=0xBFD00000 console=ttyO0,115200n8 noinitrd root=/dev/mtdblock4  rw rootfstype=jffs2 ip=dhcp eth=$(ethaddr) earlyprintk'

     

    Sorry for interrupting

    BR

    Hennessy