Other Parts Discussed in Thread: SYSBIOS
HI, this is Sangyun.
I'm studing EVM in korea.
I visit to Question for my problem.
First, I can't be using English very well.
I'm studying C6A8167(DM816x) EVM.
EVM connect linux host.
My linux host version is Ubuntu 10.04 LTS.
EVM first boots to a given state is an SD card.
I want use C6Accel in EVM include OpenCV.
The current situation,
http://processors.wiki.ti.com/index.php/Introduction_to_C6Accel
is shown in DM8148/DM8168/C6A8168 Users Minimum system requirements download.
I download these.
(Codec engine 3.x
TI CGT 7.2
Xdctools 3.2x
Linuxutils 3.21.00.01
Syslink 2.x
Xdais 7.2x
SYSBios 6.3x
Framework components 3.2x
Ipc 1.2x
Linux-psp4.00.00.07 )
and were installed on the host computer.
Order from the site was conducted during the...
Rulses.make part is difficult to fix for me.
I want know in detail.
2. Build the package by using the command make command in the root directory of the package.
in upper section I tried 'make all'.
I got 2errors in 'make server'.
Also, I got 2errors in 'make c6accel'.
Does any place in this case suspect?
I cant debug it.
And I want know 3,4,5 section.
Please explain to me in deail.
In addition, I want know how to use c6accel.
Please explain as much as possible.
Thank you.