This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDXC support on AM335x+linux platform



Hi, all

    My customer want to confirm whether AM335x+linux platform can support SDXC or not. I checked the commits in Linux kernel tree, found that there is a commit talking about SXDC as following, so can anyone help me to confirm it ?

commit f2815f68dabbb373fd1c9f0fd4a609d486697c2b
Author: Subhash Jadavani <subhashj@codeaurora.org>
Date: Wed Aug 10 11:16:01 2011 +0530

mmc: sd: Handle SD3.0 cards not supporting UHS-I bus speed mode

Here is Essential conditions to indicate Version 3.00 Card
(SD_SPEC=2 and SD_SPEC3=1) :
(1) The card shall support CMD6
(2) The card shall support CMD8
(3) The card shall support CMD42
(4) User area capacity shall be up to 2GB (SDSC) or 32GB (SDHC)
User area capacity shall be more than or equal to 32GB and
up to 2TB (SDXC)
(5) Speed Class shall be supported (SDHC or SDXC)

So even if SD card doesn't support any of the newly defined
UHS-I bus speed mode, it can advertise itself as SD3.0 cards
as long as it supports all the essential conditions of
SD3.0 cards. Given this, these type of cards should atleast
run in High Speed mode @50MHZ if it supports HS.

    But current initialization sequence for SD3.0 cards is
such that these non-UHS-I SD3.0 cards runs in Default
Speed mode @25MHz.

This patch makes sure that these non-UHS-I SD3.0 cards run
in High Speed Mode @50MHz.

Tested this patch with SanDisk Extreme SDHC 8GB Class 10 card.