Other Parts Discussed in Thread: AM3359, AM3358
Hello,
First of all, I am new to this type of development and I'm trying to follow the installation and setup instructions to boot Linux on the AM3359 EVM board we've purchased.
- Downloaded LINUXEZSDK-AM335X v5.03.03 onto my host pc which is running Ubuntu 10.04 LTS 64 bit Server
- Installed the ti-sdk-am335x-evm-05.03.03.00-Linux-x86-Install successfully
- Did the post installation e.g run setup.sh
- The above script auto detected my ip address e.g in this instant 172.17.10.156 which is connected to our LAN
- Connected the EVM serial port to /dev/ttyS0 on the Host PC
- Ensured that the Sysboot switches sw3 and sw4 were set as directed in the quick start guide
- Disconnected the cable from the host PC and our LAN and instead Connected the supplied Ethernet cable to the general purpose Ethernet socket on the EVM to the Ethernet socket on the Host PC
- The Minicom session started ok running the supplied setupBoard.minicom script
- Powered on the board within the 300 secs time (in which time Linux should have booted as stated at the end of setup.sh)
- Nothing happens in the minicom window.
I tried this several times with no luck. I know the mincom session is ok because when I booted from the supplied sd card which has the ethercat demo stuff on it, the minicom terminal showed that this was working ok.
Am I missing something fundamental here, any help, greatly appreciated.
Thanks,