Other Parts Discussed in Thread: OMAPL138
Hi,
I work on OMAPL138 and I try to operate MESSAGE_Create () function of DSPLink module and i recieve this error msg:
========== Sample Application : MESSAGE ==========
Entered MESSAGE_Create ()
dsplink driver open: /dev/dsplink: No such file or directory
PROC_setup () failed. Status = [0x80008008]
Leaving MESSAGE_Create ()
This error is in PROC_setup function in this line code: status = DRV_INITIALIZE (&DRV_handle) ;
What is the problem? Is it because DSPLink driver is not install?
How can i install DSPLink driver?
Thanks, Oded.