Other Parts Discussed in Thread: OMAPL138, OMAP-L138
I am working with LOGICPD EVM but without LCD . The usb_dev_msc not work well : the PC recognize the device but with errors
-Divice type : Other devices
-Manufacturer : Unknown
-Location : Port_#0008.Hub_#0003 -Device Status : "The drivers for this device are not installed. (Code 28) There is no driver selected for the device"
I think because this axample use/set LCD monitor that I haven't .
Is there someone that has used usb_dev_msc example without LCD monitor ?
Can you send me advise ?