This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 Video Input configuration details

Dear all,

I'm working on both TI DM814xEVM (Mistral) and our custom hardware, with EZSDK 5.03.01.15.

I would like to use the digital video input port with something like the capture_dei_encode.oms OMTB example.

However I'm wondering where some low level parameter (e.g. HSYNC/VSYNC and other control signal polarity) can be configured at OMX IL level.

I read "DM814x Openmax components user's guide" but I've found only a few parameter that the user is allow to set

Is some other detailed documentation about VFCC Index Paramters apart from the above document?

If those parameters cannot be set at OMX IL level do I have to go at a lower (M3?) level? In this case, in the next release of EZSDK will OMX IL parameter be expanded with some other configuration options?

Best Regards,

Andrea