What I use is DM8168, the EZSDK is ti-ezsdk_dm816x-evm_5_01_01_80, the linux kernel is linux/i386 2.6.37 Kernel Configuration.
When I make the menuconfig I found there is--> CIFS support(advanced network filesystem, SMBFS successor),But when I select it
as the module and recompiled the filesystem,smb service still was still not supported.
So what can I do to enable the samba service.
I have tried the transplant samba to the board. But I'm not familar with the setting args when compiling it.
Please help.
Thanks.