Other Parts Discussed in Thread: PCM3168A
Hi,now i am using the C6713 and PCM3168A to do an experiment, the BCKDA,LRCKDA and SCKI of PCM3168A are from MCASP of c6713 , BCKDA connection from ACLKX0 of MCASP,LRCKDA connection from AFSX0 of MCASP,SCKI connection from AHCLKX0 of MCASP. I want to the MCASP work at the TDM mode,but it no data out put, and the XSTAT register is 0x00000154, the XCKFAIL bit is 1(transmit clock failure did occur.). But i set the XMOD bit 0(work at burst mode)and did not modify other programs,i can detected data output. who can tell me why, who can help me ,thinks