I am a new to the omap3530 .Now I use dvsdk_wince_01_11_00_03_patch_01(download from ti web) on windows ce ,My PC eniverment is :windows XP Sp3 ,vs2005+sp1, wince6.0 ,wince6.0sp1,wince6.0sp2,wince6.0sp3 ,and wince6.0sp3 update to 2011.when I build the EVM_OMAP3530 BSP ,the project is successful,but when I buid the DVSDK(according to Install GUILD OMAP3530.pdf),it is failed. the errror is list:
(1):from c6accel and codecserver logs: "C:/ti-tools/bios/xdctools/packages/xdc/cfg/Main.xs", line 40: XDC runtime error: can't find the library 'export/BIN/DspBios/OMAP3530/OMAP3530_0/RELEASE/dsplink.lib' specified by package dsplink.dsp.
(2)from dmai logs : js: "C:/ti-tools/bios/xdctools/packages/xdc/cfg/Main.xs", line 40: XDC runtime error: can't find the library 'export/BIN/WinCE/OMAP3530/RELEASE/dsplinkapi.lib' specified by package dsplink.gpp.
(3) tne dsplink logs:
Starting ARM build
BUILD: [01:0000000111:INFO ] ===========================================================
BUILD: [01:0000000112:INFO ] gmake: *** No rule to make target `release'. Stop.
BUILD: [01:0000000113:INFO ] ===========================================================
BUILD: [01:0000000114:INFO ] Starting ARM sample application build
BUILD: [01:0000000115:INFO ] ===========================================================
BUILD: [01:0000000116:INFO ] Makefile:69: \\make\\start.mk: No such file or directory
BUILD: [01:0000000117:INFO ] gmake: *** No rule to make target `\\make\\start.mk'. Stop.
BUILD: [01:0000000118:INFO ] ===========================================================
BUILD: [01:0000000119:INFO ] Starting DSP build
BUILD: [01:0000000120:INFO ] ===========================================================
BUILD: [01:0000000121:INFO ] gmake: *** No rule to make target `release'. Stop.
BUILD: [01:0000000122:INFO ] ===========================================================
BUILD: [01:0000000123:INFO ] Starting DSP sample application build
from the errors,I know when I build the project ,I don't product the the file folders: /dsplink/gpp/export/bin , /dsplink/gpp/export/build and
/dsplink/dsp/export/bin , /dsplink/dsp/export/build
what is wrong with me ? who can help me
ths advance