Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Hello
As i've already read I am not only person having this problem. Besides of this, I could not find anyone who uses the same configuration as I am.
I have Logic omapl138 EVM, which contains of a 8MB SPI memory, and MMC/SD slot
UBL,U-boot, and linux kernel are loaded into this memory.
rootFS is loaded into SD card. (This is microSD in SD adapter)
Everything works fine, when I am using ready kernel uImage file (provided with the EVM)
When I am trying to develop my own configuration, and load the kernel into memory, I got a fallowing problem
Clock: disable unused emac
Clock: disable unused mmc
U-Boot 2009.11 (Nov 09 2010 - 18:48:43)
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.32.58
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1500940 Bytes = 1.4 MB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux............................................................................................... done, booting the kernel.
Linux version 2.6.32.58 (filip@filip-MS-7599) (gcc version 4.5.2 (Sourcery G++ Lite 2011.03-42) ) #4 PREEMPT Sun Mar 11 12:22:43 CET 2012
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DA850/OMAP-L138 EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci da850/omap-l138 variant 0x0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 8128
Kernel command line: mem=32M console=ttyS2,115200n8 root=/dev/mmcblk0p1 rw rootwait ip=off
PID hash table entries: 128 (order: -3, 512 bytes)
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory: 32MB = 32MB total
Memory: 29340KB available (2648K code, 272K data, 96K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 149.50 BogoMIPS (lpj=747520)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 144 gpio irqs
regulator: core version 0.5
NET: Registered protocol family 16
bio: create slab <bio-0> at 0
Switching to clocksource timer0_1
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
msgmni has been set to 57
io scheduler noop registered
io scheduler anticipatory registered (default)
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a 16550A
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a 16550A
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a 16550A
console [ttyS2] enabled
brd: module loaded
console [netcon0] enabled
netconsole: network logging started
i2c /dev entries driver
cpuidle: using governor ladder
cpuidle: using governor menu
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
TCP cubic registered
NET: Registered protocol family 17
Clocks: disable unused emac
Clocks: disable unused mmcsd
Waiting for root device /dev/mmcblk0p1...
Device Drivers --->
<*>MMC/SD/SDIO card support --->
[*] Assume MMC/SD cards are non-removable
static int da850_evm_mmc_get_cd(int index)
{
//return !gpio_get_value(DA850_MMCSD_CD_PIN);
return 1;
}
This also does nothing.
I am out of ideas. Please Help me.
Regards