I using the PDLogic c6748 evm borad.
I have a Problem.
TSK_sleep() is not working.
Run TKS_sleep() abort the operation.
and
PRD is not Working.
Help...Please
ccs version : 3.3.82.13
bios 5.41.11.38
code Generation : v7.0.3
xdc : 3.15.1.59
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I using the PDLogic c6748 evm borad.
I have a Problem.
TSK_sleep() is not working.
Run TKS_sleep() abort the operation.
and
PRD is not Working.
Help...Please
ccs version : 3.3.82.13
bios 5.41.11.38
code Generation : v7.0.3
xdc : 3.15.1.59
Hi Sung-min,
could you provide more information? Where are you trying to call TSK_sleep() from?
This is my code.
void main()
{
unsigned int rtn;
USTIMER_init();
I2C_init(I2C0, I2C_CLK_400K);
UART_init(DEBUG_PORT, 115200);
return;
}//end main
void Task0(void)
{
int i;
double a1=3.3, b1=2.2, c1=1.1;
while(1)
{
LED_turnOn(LED_1);
for(i=0;i<65535;i++)
{
a1=b1*c1;
b1=c1+a1;
c1=a1/b1;
}
LED_turnOff(LED_1);
TSK_sleep(100);
}
}
Task0 is working LED on/off.
Task0 is not pass TSK_sleep(100).
LED1 is ones twinkle.
HI Sung-min,
have you tried one of the shipped BIOS 5 examples? You can create a "New CCS Project" where you will find a "clk example" that uses TSK_sleep().

(Note: The snapshot was taken from CCS v5.1)