Hi
From the SPRS680B, it is given C6Integra has 6 Chipselects upto 256MB per chip select pin
so cumulatively GPMC has address space of 1536MB.
i) Can I connect 1 GB external device(NOR) to the GPMC bus, I think it is not a valid configuration because
each chipselect supports 256MB of address space. Am I correct?
ii) In the same manual(SPRS280b) section 2.9.1 L3 memory map gives only 512MB of address space for GPMC.
Can I use 6 devices using GPMC bus each supporting 256MB of address space?
Thanks in advance
Dinesh