This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP Interface w/ External DAC



We would like to use 1 McBSP port as an I2S input and another port as the I2S output. We want to feed in the master clock (either 24.57MHz or 22.7MHz depending on the sample rate of the audio). Reading through the TRM I'm a little confused about the configuration and if this is possible.