Hello,
1. I imported the FFT_Example_66_LE_COFF project into a new workspace.
According to link settings, the coff file contains only libc.a.
But according to map file the executable contains also dsplib.
Where it is in the link settings ? (and also the path to this lib)
2. Upon boot from flash I want to load an application only to cores 1,2 (out of 8). How can I do it ?
In what configuration file it is stated ?
3. What is the advantage of creating a "Group" in the debug perspective ?
Thanks,
Zvika