I am trying to run the SRIO_LoopbackDioIsrexampleproject that is included with pdk_C6670_1_0_0_17. Unfortunately the readme file in the example directory isn't very helpful.
Am I supposed to run it on just one core (i.e. core 0) or on multiple cores?
Or should it be run on two cores that are connected via sRIO (i.e. on different chips)?
Should I be setting the TEST_MULTICORE define variable?
thanks
Greg