This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error information about DM8168

0x1a4)
[<c003a308>] (do_one_initcall+0x0/0x1a4) from [<c0097440>] (sys_init_module+0x9c                                                                                                 /0x1bc)
[<c00973a4>] (sys_init_module+0x0/0x1bc) from [<c0044da0>] (ret_fast_syscall+0x0                                                                                                 /0x30)
 r7:00000080 r6:00000000 r5:0001b398 r4:400aebe0
---[ end trace 6745665cf0040e10 ]---
notify_send_event failed! status = 0xfffffff3
------------[ cut here ]------------
WARNING: at drivers/dsp/syslink/omap_notify/notify.c:776 notify_send_event+0xd4/                                                                                                 0x26c()
Modules linked in: vpss(+) ipv6
Backtrace:
[<c0048b58>] (dump_backtrace+0x0/0x110) from [<c036b8d8>] (dump_stack+0x18/0x1c)
 r7:00000000 r6:c02aa1e0 r5:c04692ef r4:00000308
[<c036b8c0>] (dump_stack+0x0/0x1c) from [<c006bd54>] (warn_slowpath_common+0x54/                                                                                                 0x6c)
[<c006bd00>] (warn_slowpath_common+0x0/0x6c) from [<c006bd90>] (warn_slowpath_nu                                                                                                 ll+0x24/0x2c)
 r9:c2f2f0c0 r8:00000001 r7:00000002 r6:00000000 r5:00000009
r4:00000000
[<c006bd6c>] (warn_slowpath_null+0x0/0x2c) from [<c02aa1e0>] (notify_send_event+                                                                                                 0xd4/0x26c)
[<c02aa10c>] (notify_send_event+0x0/0x26c) from [<bf068aa0>] (vps_fvid2_init+0x1                                                                                                 64/0x490 [vpss])
[<bf06893c>] (vps_fvid2_init+0x0/0x490 [vpss]) from [<bf0680c0>] (vps_probe+0x60                                                                                                 /0x160 [vpss])
[<bf068060>] (vps_probe+0x0/0x160 [vpss]) from [<c01e0758>] (platform_drv_probe+                                                                                                 0x20/0x24)
 r7:c2400080 r6:bf0767d8 r5:c04b3c28 r4:c04b3c28
[<c01e0738>] (platform_drv_probe+0x0/0x24) from [<c01df6c4>] (driver_probe_devic                                                                                                 e+0xd0/0x190)
[<c01df5f4>] (driver_probe_device+0x0/0x190) from [<c01df7ec>] (__driver_attach+                                                                                                 0x68/0x8c)
 r7:c2400080 r6:bf0767d8 r5:c04b3c5c r4:c04b3c28
[<c01df784>] (__driver_attach+0x0/0x8c) from [<c01dee70>] (bus_for_each_dev+0x50                                                                                                 /0x84)
 r7:c2400080 r6:bf0767d8 r5:c01df784 r4:00000000
[<c01dee20>] (bus_for_each_dev+0x0/0x84) from [<c01df4e8>] (driver_attach+0x20/0                                                                                                 x28)
 r6:bf0767d8 r5:bf0767c4 r4:00000000
[<c01df4c8>] (driver_attach+0x0/0x28) from [<c01de748>] (bus_add_driver+0xb4/0x2                                                                                                 34)
[<c01de694>] (bus_add_driver+0x0/0x234) from [<c01dfb24>] (driver_register+0xb0/                                                                                                 0x13c)
[<c01dfa74>] (driver_register+0x0/0x13c) from [<c01e0a44>] (platform_driver_regi                                                                                                 ster+0x4c/0x60)
 r9:c263e000 r8:bf07c000 r7:40037000 r6:0001b398 r5:bf0767c4
r4:00000000
[<c01e09f8>] (platform_driver_register+0x0/0x60) from [<c01e0a78>] (platform_dri                                                                                                 ver_probe+0x20/0x70)
[<c01e0a58>] (platform_driver_probe+0x0/0x70) from [<bf07c030>] (vps_init+0x30/0                                                                                                 x5c [vpss])
 r5:bf076b44 r4:00000000
[<bf07c000>] (vps_init+0x0/0x5c [vpss]) from [<c003a3d8>] (do_one_initcall+0xd0/                                                                                                 0x1a4)
[<c003a308>] (do_one_initcall+0x0/0x1a4) from [<c0097440>] (sys_init_module+0x9c                                                                                                 /0x1bc)
[<c00973a4>] (sys_init_module+0x0/0x1bc) from [<c0044da0>] (ret_fast_syscall+0x0                                                                                                 /0x30)
 r7:00000080 r6:00000000 r5:0001b398 r4:400aebe0
---[ end trace 6745665cf0040e11 ]---
notify_send_event failed! status = 0xfffffff3
VPSS_CORE : Failed to init fvid2 interface,
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver

 

however,linux system can start after output error information above 。

help me,tks.

  • Hi,

    You have not initialized your bootargs with "notifyk.vpssm3_sva"

    Regards,

    Hardik Shah

  • Thank you for your reply,and I have change the bootargs,now the following is my 'bootargs'

    bootargs=console=ttyO2,115200n8 root=/dev/mtdblock7 rw rootfstype=jffs2 mem=100M earlyprintk notifyk.vpssm3_sva=0xA0000000

     

    but I always have error information as following

     

    notify_send_event failed! status = 0xfffffff0
    notify_shm_drv_sendevent failed! status = 0xfffffff0
    notify_send_event failed! status = 0xfffffff0
    notify_shm_drv_sendevent failed! status = 0xfffffff0
    notify_send_event failed! status = 0xfffffff0
    notify_shm_drv_sendevent failed! status = 0xfffffff0
    notify_send_event failed! status = 0xfffffff0
    notify_shm_drv_sendevent failed! status = 0xfffffff0
    notify_send_event failed! status = 0xfffffff0
    notify_shm_drv_sendevent failed! status = 0xfffffff0
    notify_send_event failed! status = 0xfffffff0
    notify_shm_drv_sendevent failed! status = 0xfffffff0
    notify_send_event failed! status = 0xfffffff0
    notify_shm_drv_sendevent failed! status = 0xfffffff0
    notify_send_event failed! status = 0xfffffff0
    notify_shm_drv_sendevent failed! status = 0xfffffff0
    notify_send_event failed! status = 0xfffffff0
    notify_shm_drv_sendevent failed! status = 0xfffffff0
    notify_send_event failed! status = 0xfffffff0

     

    and when I insmod vpss.ko ,the error information

     

  • and when I insmod vpss.ko ,the error information will appear above.

    so,what can I do for this ?

    best regard to you

  • You can never "just" insmod vpss without arguments. It always needs arguments when it is loaded. Try looking at board-support/media-controller-utils_2_03_01_14/src/linux/ti816x/load-hd-firmware.sh in the EZSDK.

    Ralph