This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Support for SCCB in DM3715 I2C

Hi,

I am working on a project with DM37x processor and is trying to interface Omni Vision 2659 module. Ov2659 supports SCCB interface which is a variant of I2C and we are seeing that there is no ACK in SCCB interface. Found that DM37x processor specifically supports this mode, but Linux I2C driver does not this at present. We are using Android 2.3.4 based on Linux kernel 2.6.37.

1. Would like to know if there is any support for SCCB in Linux I2C driver for this processor, if it is available as a patch or any reference source code also will be helpful

2. Does any one have Ov2659 camera sensor driver which can be shared?

Thanks in advance.

Regards,

Nandan