This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OpenCV on OMAP : any news?

Other Parts Discussed in Thread: OMAPL138, OMAP3530

Hi everyone,

Already put this question in other thread (http://e2e.ti.com/support/embedded/bios/f/355/t/167714.aspx#625052), but this secion seems to best fit my argument.

I'm looking for OpenCV acceleration using ARM + C674x floating point DSP, it will run on OMAP-L138.

I'm very interested in prerelease opencv 2.3 port discussed on this forum: how to achieve it?

I have also an Igep board with OMAP3530, then fixedpoint C64x, is there a port fot this?

I would want tu run a sample code to benchmark these two platform in OpenCV application: I 've already code written for x86 and  i want the less effort to reuse it.

Which is the right and convenient way to interoperate ARM (running some Linux ) and DSP ? C6Accel?

Is there a better forum section to discuss about my application?

Thank you!!

  • OpenCV in ARM +DSP is currently supported only on DM81XX devices using the C6Accel tool but can ported to the OMAPL138 and OMAP3530. For questions on this you may write to the C6accel software developers list mentioned here:

    http://processors.wiki.ti.com/index.php/C6EZAccel#Developer_Mailing_List

    When you write to the developers list, could you provide us some details of the end applications where you wish to utilize openCV functions on OMAPL138 and the OpenCV functions that you wish to use in your embedded application. Also could you provide the name of the local TI contact, who is supporting you.

    Regards,

    Rahul