Hi,
One of the commits[1] related to CPSW linux driver are mentioning that there is HW issue with CPSW interrupts and linux driver is using timers to workaround this. However details about this issue are not described in public errata.
Can somebody provide a bit more details about this issue?
Does it affect operation of device when pacing is disabled and CPSW RX and TX interrupts are used?
My observation so far is that interrupts stop working when I reset CPDMA even with pacing disabled.
Thanks,
Damjan
[1] http://arago-project.org/git/projects/linux-am33x.git?p=projects/linux-am33x.git;a=commit;h=8c32c4f2798e652d51920bfdd9d5ad32be68f565