I am looking to create a new CCSv5 project using the "SYS/BIOS, Typical" project template. I am using the LogicPD DM3730 Torpedo development kit. I have code running in the DSP and ARM cores now, but I need to add SYS/BIOS to the DSP side in order to utilize features of DSP Link / SYS Link for interfacing.
In CCSv5, I setup the device correctly (Family: C6000 | Variant: DM3730 | Connection: XDS100v2), but the subsequent "RTSC Configuration Settings" dialog shows no available platforms. I am not sure how to best proceed from here... Do I have to create a new platform, download one, or abandon my attempts to use any of the project templates in CCSv5? How can I get SYS/BIOS running under the hood of my existing image processing code? Thanks in advance!