Other Parts Discussed in Thread: TPS65910A, SN74LVC16245A
Hi all,
I had a look in the schematic of the AM335X EVM 15x15 Baseboard and i noticed that the NAND Flash was supplied by VDDSHV1= VAUX2= 3.3V ( TPS65910A: BOOT1=1, BOOT0 = eeprom sequence) but not mount !!
What is the reason exactly ? mount only if we use the Baseboard alone to test boot from NAND ?
On the daugher board i noticed that NOR & NAND Flash were populated with 16bits dual voltage transceivers ?
Why did you use dual voltage transceivers ?
Indeed if the VDDSHV1=VDDSHV6= VAUX2= 3.3V,a SN74LVC16245A can also be used.
By the way what is the status about booting from the NOR Flash ?
On the other hand the EEPROM sequence is not very well detailed expected in the TPS65910Ax User's Guide For AM335x Processors.
Where could i find more info about this mode ?
Thanks in advance
greg