This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

timer loop kernel oops




Hi,

i think i have the same Error (http://e2e.ti.com/support/dsp/sitara_arm174_microprocessors/f/416/t/113593.aspx#628790). The problem can be triggert bei using
this command:  cangen can0 -g 100 -I 42A -L 1 -D i -v -v
it sends CAN messages with increment payload every 100ms.

!!new info: same bug with:  watch -n 1 echo "test"


Kernel from TI am33x git repository (3.1.0) on Beaglebone platform.
After a while ~30min the Kernel throws these Ooops:

[ 9725.943072] Unable to handle kernel paging request at virtual address e9e31034
[ 9725.950629] pgd = ce844000
[ 9725.953454] [e9e31034] *pgd=00000000
[ 9725.957198] Internal error: Oops: 5 [#1]
[ 9725.961293] Modules linked in:
[ 9725.964494] CPU: 0 Not tainted (3.1.0-00010-g66bfbd2-dirty #3)
[ 9725.970973] PC is at omap2_gp_timer_set_next_event+0x14/0x74
[ 9725.976899] LR is at clockevents_program_event+0xc0/0x130
[ 9725.982543] pc : [<c0022a28>] lr : [<c0066fa8>] psr: 60000193
[ 9725.982553] sp : c05b5d30 ip : c05b5d40 fp : c05b5d3c
[ 9725.994540] r10: c050ccc0 r9 : 000008d8 r8 : 7f338790
[ 9725.999998] r7 : 0003a599 r6 : 373bf910 r5 : 00000000 r4 : 0097f3f0
[ 9726.006817] r3 : c0609d70 r2 : e9e31034 r1 : c05bd600 r0 : 0003a599
[ 9726.013639] Flags: nZCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment kernel
[ 9726.021367] Control: 10c5387d Table: 8e844019 DAC: 00000015
[ 9726.027369] Process swapper (pid: 0, stack limit = 0xc05b42f0)
[ 9726.033463] Stack: (0xc05b5d30 to 0xc05b6000)
[ 9726.038018] 5d20: c05b5d64 c05b5d40 c0066fa8 c0022a20
[ 9726.046568] 5d40: c05bd600 00000000 00000001 c05b5d88 7f338790 000008d8 c05b5dbc c05b5d68
[ 9726.055118] 5d60: c0067908 c0066ef4 7f338790 000008d8 c05d61e0 0098967f 000008d8 7fcb7b80
[ 9726.063670] 5d80: 7f338790 000008d8 7f338790 000008d8 c020d3d8 c05b5e18 c05d5bc8 c05d5c70
[ 9726.072220] 5da0: 00000003 7fcb7b80 00000001 000008d8 c05b5dd4 c05b5dc0 c0067a88 c00678ac
[ 9726.080772] 5dc0: 00000000 c05d5bc8 c05b5e4c c05b5dd8 c005c6a4 c0067a68 7f3308ed 000008d8
[ 9726.089322] 5de0: cfa6c340 7fffffff ffffffff 00000000 00000000 00000000 7f3308ed 000008d8
[ 9726.097872] 5e00: 7f3308ed 000008d8 7fcb7b80 000008d8 7f3308ed 000008d8 7f3308ed 000008d8
[ 9726.106421] 5e20: 000025fd c05bd700 00000043 00000000 00000000 00000043 c06291a4 c05d805c
[ 9726.114972] 5e40: c05b5e5c c05b5e50 c0022a0c c005c558 c05b5e94 c05b5e60 c0073dc0 c00229e4
[ 9726.123522] 5e60: 00000000 00000000 000008d8 c05d805c 00000043 00000000 c05b5f3c 80004059
[ 9726.132072] 5e80: 413fc082 00000000 c05b5eac c05b5e98 c0073f40 c0073d78 c05d805c 00000043
[ 9726.140622] 5ea0: c05b5ec4 c05b5eb0 c00762c8 c0073f1c c05e63ac 00000043 c05b5ed4 c05b5ec8
[ 9726.149172] 5ec0: c0073a28 c007624c c05b5ef4 c05b5ed8 c0016018 c00739fc c00297e8 80000013
[ 9726.157722] 5ee0: fa200000 c05b5f3c c05b5f04 c05b5ef8 c0008390 c0015fec c05b5f74 c05b5f08
[ 9726.166273] 5f00: c0014cf4 c000838c ba846e68 0000aebc 386d697e 0000aebc 00000000 c05bdf30
[ 9726.174823] 5f20: c063b1b0 00000000 80004059 413fc082 00000000 c05b5f74 386d697e c05b5f50
[ 9726.183373] 5f40: c00629b4 c00297e8 80000013 ffffffff 386d697e 0000aebc 386d697e 0000991e
[ 9726.191923] 5f60: 413fc082 c05bdf20 c05b5f9c c05b5f78 c030eb90 c0029790 c05b4000 c0609684
[ 9726.200473] 5f80: c05baf2c c05baf24 80004059 413fc082 c05b5fbc c05b5fa0 c00167f4 c030ead8
[ 9726.209023] 5fa0: c05b692c c05a5004 c05a4fd4 c05baf24 c05b5fcc c05b5fc0 c041a9a4 c0016798
[ 9726.217577] 5fc0: c05b5ff4 c05b5fd0 c057a7f8 c041a93c c057a32c 00000000 00000000 c05a5004
[ 9726.226128] 5fe0: 10c53c7d c05b6040 00000000 c05b5ff8 8000803c c057a588 00000000 00000000
[ 9726.234668] Backtrace:
[ 9726.237242] [<c0022a14>] (omap2_gp_timer_set_next_event+0x0/0x74) from [<c0066fa8>] (clockevents_program_event+0xc0/0x130)
[ 9726.248794] [<c0066ee8>] (clockevents_program_event+0x0/0x130) from [<c0067908>] (tick_dev_program_event+0x68/0x174)
[ 9726.259788] r9:000008d8 r8:7f338790 r7:c05b5d88 r6:00000001 r5:00000000
[ 9726.266628] r4:c05bd600
[ 9726.269380] [<c00678a0>] (tick_dev_program_event+0x0/0x174) from [<c0067a88>] (tick_program_event+0x2c/0x34)
[ 9726.279669] [<c0067a5c>] (tick_program_event+0x0/0x34) from [<c005c6a4>] (hrtimer_interrupt+0x158/0x2f8)
[ 9726.289583] [<c005c54c>] (hrtimer_interrupt+0x0/0x2f8) from [<c0022a0c>] (omap2_gp_timer_interrupt+0x34/0x3c)
[ 9726.299960] [<c00229d8>] (omap2_gp_timer_interrupt+0x0/0x3c) from [<c0073dc0>] (handle_irq_event_percpu+0x54/0x1a4)
[ 9726.310874] [<c0073d6c>] (handle_irq_event_percpu+0x0/0x1a4) from [<c0073f40>] (handle_irq_event+0x30/0x40)
[ 9726.321064] [<c0073f10>] (handle_irq_event+0x0/0x40) from [<c00762c8>] (handle_level_irq+0x88/0xf0)
[ 9726.330575] r5:00000043 r4:c05d805c
[ 9726.334355] [<c0076240>] (handle_level_irq+0x0/0xf0) from [<c0073a28>] (generic_handle_irq+0x38/0x44)
[ 9726.344047] r5:00000043 r4:c05e63ac
[ 9726.347838] [<c00739f0>] (generic_handle_irq+0x0/0x44) from [<c0016018>] (handle_IRQ+0x38/0x8c)
[ 9726.356996] [<c0015fe0>] (handle_IRQ+0x0/0x8c) from [<c0008390>] (asm_do_IRQ+0x10/0x14)
[ 9726.365409] r7:c05b5f3c r6:fa200000 r5:80000013 r4:c00297e8
[ 9726.371391] [<c0008380>] (asm_do_IRQ+0x0/0x14) from [<c0014cf4>] (__irq_svc+0x34/0xa0)
[ 9726.379716] Exception stack(0xc05b5f08 to 0xc05b5f50)
[ 9726.385030] 5f00: ba846e68 0000aebc 386d697e 0000aebc 00000000 c05bdf30
[ 9726.393636] 5f20: c063b1b0 00000000 80004059 413fc082 00000000 c05b5f74 386d697e c05b5f50
[ 9726.402237] 5f40: c00629b4 c00297e8 80000013 ffffffff
[ 9726.407575] [<c0029784>] (am33xx_enter_idle+0x0/0x94) from [<c030eb90>] (cpuidle_idle_call+0xc4/0x138)
[ 9726.417360] r4:c05bdf20
[ 9726.420034] [<c030eacc>] (cpuidle_idle_call+0x0/0x138) from [<c00167f4>] (cpu_idle+0x68/0xb0)
[ 9726.428997] r9:413fc082 r8:80004059 r7:c05baf24 r6:c05baf2c r5:c0609684
[ 9726.435885] r4:c05b4000
[ 9726.438665] [<c001678c>] (cpu_idle+0x0/0xb0) from [<c041a9a4>] (rest_init+0x74/0x78)
[ 9726.446805] r7:c05baf24 r6:c05a4fd4 r5:c05a5004 r4:c05b692c
[ 9726.452803] [<c041a930>] (rest_init+0x0/0x78) from [<c057a7f8>] (start_kernel+0x27c/0x2d0)
[ 9726.461502] [<c057a57c>] (start_kernel+0x0/0x2d0) from [<8000803c>] (0x8000803c)
[ 9726.469286] Code: e92dd800 e24cb004 e59f305c e5932028 (e5922000)
[ 9726.475743] ---[ end trace 360b6b0f468e4aa2 ]---
[ 9726.480603] Kernel panic - not syncing: Fatal exception in interrupt
[ 9726.487299] Backtrace:
[ 9726.489890] [<c0018b70>] (dump_backtrace+0x0/0x10c) from [<c0424a00>] (dump_stack+0x18/0x1c)
[ 9726.498762] r7:00000001 r6:c0022a2a r5:c060a5a0 r4:c060a5a0
[ 9726.504742] [<c04249e8>] (dump_stack+0x0/0x1c) from [<c0424a68>] (panic+0x64/0x198)
[ 9726.512801] [<c0424a04>] (panic+0x0/0x198) from [<c0018ed4>] (die+0x258/0x2bc)
[ 9726.520393] r3:00010000 r2:c05b5b58 r1:00000209 r0:c04f28f0
[ 9726.526378] [<c0018c7c>] (die+0x0/0x2bc) from [<c001b60c>] (__do_kernel_fault+0x6c/0x8c)
[ 9726.534897] [<c001b5a0>] (__do_kernel_fault+0x0/0x8c) from [<c001b874>] (do_bad_area+0x48/0x74)
[ 9726.544042] r9:000008d8 r8:7f338790 r7:8e844019 r6:00000000 r5:c0004000
[ 9726.550928] r4:60000193
[ 9726.553695] [<c001b82c>] (do_bad_area+0x0/0x74) from [<c001b904>] (do_translation_fault+0x64/0xa8)
[ 9726.563113] r4:00000005
[ 9726.565789] [<c001b8a0>] (do_translation_fault+0x0/0xa8) from [<c00085c8>] (do_DataAbort+0x3c/0xa4)
[ 9726.575300] r7:c05b5ce8 r6:e9e31034 r5:c05bb3a4 r4:00000005
[ 9726.581282] [<c000858c>] (do_DataAbort+0x0/0xa4) from [<c0014c98>] (__dabt_svc+0x38/0x60)
[ 9726.589880] Exception stack(0xc05b5ce8 to 0xc05b5d30)
[ 9726.595196] 5ce0: 0003a599 c05bd600 e9e31034 c0609d70 0097f3f0 00000000
[ 9726.603802] 5d00: 373bf910 0003a599 7f338790 000008d8 c050ccc0 c05b5d3c c05b5d40 c05b5d30
[ 9726.612403] 5d20: c0066fa8 c0022a28 60000193 ffffffff
[ 9726.617710] r7:c05b5d1c r6:ffffffff r5:60000193 r4:c0022a28
[ 9726.623696] [<c0022a14>] (omap2_gp_timer_set_next_event+0x0/0x74) from [<c0066fa8>] (clockevents_program_event+0xc0/0x130)
[ 9726.635322] [<c0066ee8>] (clockevents_program_event+0x0/0x130) from [<c0067908>] (tick_dev_program_event+0x68/0x174)
[ 9726.646385] r9:000008d8 r8:7f338790 r7:c05b5d88 r6:00000001 r5:00000000
[ 9726.653269] r4:c05bd600
[ 9726.656040] [<c00678a0>] (tick_dev_program_event+0x0/0x174) from [<c0067a88>] (tick_program_event+0x2c/0x34)
[ 9726.666386] [<c0067a5c>] (tick_program_event+0x0/0x34) from [<c005c6a4>] (hrtimer_interrupt+0x158/0x2f8)
[ 9726.676366] [<c005c54c>] (hrtimer_interrupt+0x0/0x2f8) from [<c0022a0c>] (omap2_gp_timer_interrupt+0x34/0x3c)
[ 9726.686804] [<c00229d8>] (omap2_gp_timer_interrupt+0x0/0x3c) from [<c0073dc0>] (handle_irq_event_percpu+0x54/0x1a4)
[ 9726.697790] [<c0073d6c>] (handle_irq_event_percpu+0x0/0x1a4) from [<c0073f40>] (handle_irq_event+0x30/0x40)
[ 9726.708044] [<c0073f10>] (handle_irq_event+0x0/0x40) from [<c00762c8>] (handle_level_irq+0x88/0xf0)
[ 9726.717555] r5:00000043 r4:c05d805c
[ 9726.721332] [<c0076240>] (handle_level_irq+0x0/0xf0) from [<c0073a28>] (generic_handle_irq+0x38/0x44)
[ 9726.731026] r5:00000043 r4:c05e63ac
[ 9726.734805] [<c00739f0>] (generic_handle_irq+0x0/0x44) from [<c0016018>] (handle_IRQ+0x38/0x8c)
[ 9726.743962] [<c0015fe0>] (handle_IRQ+0x0/0x8c) from [<c0008390>] (asm_do_IRQ+0x10/0x14)
[ 9726.752376] r7:c05b5f3c r6:fa200000 r5:80000013 r4:c00297e8
[ 9726.758358] [<c0008380>] (asm_do_IRQ+0x0/0x14) from [<c0014cf4>] (__irq_svc+0x34/0xa0)
[ 9726.766682] Exception stack(0xc05b5f08 to 0xc05b5f50)
[ 9726.771997] 5f00: ba846e68 0000aebc 386d697e 0000aebc 00000000 c05bdf30
[ 9726.780603] 5f20: c063b1b0 00000000 80004059 413fc082 00000000 c05b5f74 386d697e c05b5f50
[ 9726.789204] 5f40: c00629b4 c00297e8 80000013 ffffffff
[ 9726.794527] [<c0029784>] (am33xx_enter_idle+0x0/0x94) from [<c030eb90>] (cpuidle_idle_call+0xc4/0x138)
[ 9726.804312] r4:c05bdf20
[ 9726.806986] [<c030eacc>] (cpuidle_idle_call+0x0/0x138) from [<c00167f4>] (cpu_idle+0x68/0xb0)
[ 9726.815948] r9:413fc082 r8:80004059 r7:c05baf24 r6:c05baf2c r5:c0609684
[ 9726.822832] r4:c05b4000
[ 9726.825600] [<c001678c>] (cpu_idle+0x0/0xb0) from [<c041a9a4>] (rest_init+0x74/0x78)
[ 9726.833741] r7:c05baf24 r6:c05a4fd4 r5:c05a5004 r4:c05b692c
[ 9726.839726] [<c041a930>] (rest_init+0x0/0x78) from [<c057a7f8>] (start_kernel+0x27c/0x2d0)
[ 9726.848425] [<c057a57c>] (start_kernel+0x0/0x2d0) from [<8000803c>] (0x8000803c)