This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Booting from XIP (NOR-Flash): Address lines A12-A27

Hello,

at the TRM (SPRUH73C) chapter 26.1.7.2.2 is mentioned:

Specifically, external logic is needed to isolate the upper address lines (A12–A27) of the NOR flash from the device pins and drive them low during boot. Once the initial software starts running, it can appropriately configure the pinmux setting for the lines and remove the isolation to allow GPMC to drive all the address lines.

May I ask some questions?

  • What is meant with external logic? Driving the address lines A12-A27 of NOR-Flash low with pull down resistors via bus switch (e.g. LVC16244)?
  • With which pin of AM335x should I use for releasing the switches after first boot-up?
  • Do you have some kind of reference schematics that do not harm rise and fall times or timing requirements for NOR Flash communication?
  • How many nanoseconds maximium the external logic could consume?

Best regards,

Martin