This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6457L support with latest CCS (CCS5.1.1.00033_linux)

For some reason, latest CCS, available to download, can't work with EVM TMDSEVM6457L, using default configuration file evmc6457l.xml.

"Connect Target" operation always return with error.

Unfortunately, method, recommended here http://processors.wiki.ti.com/index.php/BiosMulticoreSDK_1.0_GettingStartedGuide#5._Use_JTAG_to_Load_the_Application

doesn't work also. CCS doesn't recognize configuration file, copied from MSDK.

I checked configuration file and did some changes in it. Actually, I had to change 2 ids inside.

Hope this help.

Dmitry.