This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

816X EVM Ethernel Activity LED



Hi,

I've noticed that only one of the two LEDs on the 816X EVM RJ45 Ethernet jack are working.  The one LED that is working must be a link LED because it turns on when an Ethernet cable is connected to the EVM.  I would expect the other LED to flash when there is Ethernet activity, but it is always off.

How can I get the other LED to flash when there is Ethernet activity?

Paul