This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCIe boot: C6678 reset problem



Our application is initially loaded via PCIe. That means we have a working primary i2c boot, followed by a secondary PCIe boot. The host can then upload the software to the DSP and run it. That works fine.

However, the host initiated reset is a problem. The host has GPIO connected pins to the reset inputs (soft, hard (RESETFULL) and local resets but we cannot use POR because that is shared between different components on our board!) of the DSP.

After reset is given, the DSP is expected to rerun the bootloader and follow the exact same sequence as on a POR except for polling the DEVSTAT register pins. After the host has restored the PCIe configuration of the DSP, I can again upload software (and write/read registers across PCIe) to the DSP, but this newly uploaded software never runs.

In another thread, I read that someone was able to reset the DSP via PCIe commands (although not recommended or supported because of PLL issues). I also succeeded in doing just that: resetting (soft reset or hard reset) the DSP by just writing registers across PCIe but the outcome is the same. After reset, I can upload new software, but it does not run.

What is missing here?

Or has the DSP not come out of reset correctly?

Is the POR required for this feature?

  • Hi Gert, I think that old thread was started by me.

    We are able to reset over PCIe by writing to the PLL Reset register, and we do this all the time.

    You must do this:

    Enable MST_PRIV bit in PCIE_PRIORITY_REG from the host (otherwise key below wont be accepted and nothing will happen).

    Write the proper key value (0x5A69 i think) to the PLL_RSTCNTL register. Check that the key was accepted, by reading back, I think it should be 0x000C. This step can easily go wrong.

    Request the reset via PL_RSTCNTL register.

    After the reset, I suggest connecting to the C6678 using CCS, and check that Core 0 has re-entered the IBL (probably addresses 0x00800000 to 0x0081FFFF) and is polling the Boot Magic Address.

    Best wishes, Jonathan

     

  • Hi Jonathan,

    yes, I read your great tip about PCIe host driven reset.

    To clarify my question:

    Reset is working.

    In short the local DSP procedure is...

    volatile unsigned int* pE8 = (volatile unsigned int*) (0x023100E8);

    volatile unsigned int* pEC = (volatile unsigned int*) (0x023100EC);

    volatile unsigned int nE8 = *pE8;

    volatile unsigned int Key = 0x5A69;

    *pE8 = Key;

    *pEC |= ((1 << 12) | (1 << 13)); // set as soft reset, standard would be hard reset

    *pE8 = Key;

    *pE8 = 0; // reset

    To summarize, in order to enable MST, via PCIe...

    • unsigned int* p_mapped points to the TI DSP 4K config section.

    • and #define TI_PCIE_PRIORITY 0x3C //3Ch Section 3.1.14

    • volatile unsigned int* pRegister;

    if (do_enableprivilege)

    { // this enables privileged writes initiated by PCIe

    unsigned int bit = (0x1<<16);

    pRegister = (unsigned int *) ( ((unsigned int) p_mapped) + TI_PCIE_PRIORITY);

    *pRegister = SWAP(bit); // Big endian host to Little endian DSP

    }

    After, that the 0x02310000 registers can be mapped via PCIe and the same procedure as the local running reset function can be performed.

    I checked and IBL is restarted at PC 0x20B00000, both for local running reset, or PCIe remotely triggered reset.

    The same thing happens when the (not POR) reset pins are toggled. However, in both cases the software upload procedure has not the desired outcome.

    PCIe seems to be OK after the reset: I can peek and poke memory in the DSP from the host. Upload is working; I need to verify whether it starts (as triggered by Host) or not. So, I will need to debug that further and check whether it leaves the IBL and attempts to run the uploaded software.

    I was just wondering what could prevent the software from running again, especially taking into account that the upload procedure works the first time.

  • following experiment done:

    • host stores PCIe BAR config in file
    • host resets C6678 via reset pin
    • host restores PCIe BAR config from file
    • host uploads software to DSP
    • a check program on host reveals software is not running on the DSP.
    • Debugger connected, it shows DSP still running IBL; I manually set the PC to 0x00800000 -> then run -> the software runs correctly as checked by host.

    Note: The programmed magic boot address for core 0 was correct and was thus 0x10800000.

    The code snippet to get the DSP out of reset is as follows:

        /* Now poke the legacy interrupt on the EP to have it break out of boot.
        Do it twice just to be sure */
        if (do_prints) printf("set registers... trigger INT\n");
        pRegister = (unsigned int *) ( ((unsigned int) p_mapped) + TI_MSI_IRQ);
        *pRegister = SWAP(0xff00); /*    This register is written to by the remote device. Writes initiated by an EP over PCIe link that target
                                        BAR0 of the RC land to this register if the offset matches. To generate MSI Interrupt 0, the EP should
                                        write 0x0000_0000 to this register. It will result in a pulse on bit zero triggering the MSI interrupt
                                        from PCIESS to the external processor. */
        if (do_prints) printf("set registers... trigger INT..DONE1\n");
        *pRegister = SWAP(0xff00);
        if (do_prints) printf("set registers... trigger INT..DONE2\n");

    My current work hypothesis is that the IBL is not triggered correctly to start the program at the magic_boot_address.

  • Are you using RESETFULL or RESETZ. You need either RESETFULL or POR to trigger the complete boot loader process.

    Thanks,

    Arun.

  • RESETFULL is used.

    Best regards,

    Gert.

  • Are you still poking the boot magic address and sending the MSI interrupts after you load the program right?

    thanks,

    Arun

  • Yes, exact same procedure as on a first-time upload.

  • This is strange. Where is the PC after you loaded the program through PCIe? Also see if there is the devstat register value is different between the two cases.

    thanks,

    arun

  • Gert,

    One more thing to mention is the that only the sticky bits in the PCIe memory-mapped registers (MMRs) will be retained (most of them will be reset to default values) after the soft reset (RESETFULL). The description in the data manuals will be revised in the next release.

    That means you need to re-program the applications registers (e.g. address translation, interrupt setup) and configuration registers (e.g. BARs) after the reset.

    So you should check if the host could indeed trigger the MSI interrupt in PCIe and wake up the Core0 for boot_magic_address.

    Sincerely,

    Steven

  • There is indeed a difference between the interrupt registers on a first and second software upload. Considering the order in the boot process: first I2C, then PCIe, then the IBL waits for the interrupt + magic boot address. Should the IBL not have set the interrupt registers in the correct state?

    I will now try to manually set the registers in the same state as on a first upload, then check whether the interrupt can be triggered and whether the IBL transfers the PC to the magic boot address.

  • I reprogrammed the interrupt registers so that they are identical to a first upload status; but to no avail.

    According to SPRUGY5A—September 2011, page 28:

    "If the I2C EEPROM is used to configure the PCI registers, the BAR configurations are
    driven by the parameter table downloaded through I2C. On the boot reentry, the PCIe
    boot code is executed with these BAR configurations. In this mode of operation, the I2C
    peripheral is also configured by the bootloader.
    The bootloader code also configures the interrupt subsystem by configuring the
    chip-level interrupt controller, then executes the IDLE instruction (Mostly MSI or
    legacy interrupts can be used). After the host transfers the boot table directly to the
    memory location and if the BOOT MAGIC ADDRESS register is non-zero, the ROM
    code copies the start address of the application from the BOOT MAGIC ADDRESS to
    the program counter wakes up the DSP through an interrupt generated by poking the
    MSI application register and executes the application loaded. If the BOOT MAGIC
    ADDRESS register is still zero the ROM code keeps the DSP in idle till the value is
    non-zero."

    So the IBL configures the interrupt subsystem? That clearly has not happened here. Am I looking at a real reset problem?

    DEVSTAT register reads in both scenarios 0x0001000B

    Can I force a local reset on core 0 to start software at L2SRAM?

  • Hi Jonathan,

    I have a question for you: Are uploading your software via PCIe or are you using e.g. FLASH ?

    Hi All, :-)

    I have here the register dump taken at the time right after the second software upload (after the reset).

    IBL code is running PC@0x20B01270, which is disassembled into the 'IDLE' instruction.

    What we don't know is whether the I2C part has run to completion. The I2C part initializes the DDR3 RAM and performs the PLL fix.

    I can read/write the DDR3 RAM via PCIe at this stage. So, it seems I2C did run. Then IBL PCIe initialization should have been performed.

    Since the host can talk to the DSP via PCIe, this probably has also run.

    Core Registers    Core Registers    
        PC    0x20B01270    Core Register    
        CLK    0x00000000    Core Register    
        SP    0x0087FFA0    Core Register    
        FP    0x0087FFA0    Core Register    
        A0    0x00000001    Core Register    
        A1    0x00000001    Core Register    
        A2    0x01000000    Core Register    
        A3    0x01000000    Core Register    
        A4    0x01845044    Core Register    
        A5    0x20000000    Core Register    
        A6    0x00000018    Core Register    
        A7    0x00000000    Core Register    
        A8    0x21800004    Core Register    
        A9    0x20B09A80    Core Register    
        A10    0x000003F0    Core Register    
        A11    0x0087FFFC    Core Register    
        A12    0x02320010    Core Register    
        A13    0x00873700    Core Register    
        A14    0x00873680    Core Register    
        A15    0x008734A8    Core Register    
        A16    0x00000000    Core Register    
        A17    0x002625A0    Core Register    
        A18    0x0002625A    Core Register    
        A19    0x00000000    Core Register    
        A20    0x00000000    Core Register    
        A21    0x00EE6B28    Core Register    
        A22    0x00873680    Core Register    
        A23    0x0040202C    Core Register    
        A24    0x00000010    Core Register    
        A25    0x0081D5CC    Core Register    
        A26    0x0081D5CC    Core Register    
        A27    0x00000001    Core Register    
        A28    0x00000000    Core Register    
        A29    0x0081EFCC    Core Register    
        A30    0x00000001    Core Register    
        A31    0x00000000    Core Register    
        B0    0x21000001    Core Register    
        B1    0x20000001    Core Register    
        B2    0x00000000    Core Register    
        B3    0x20B01264    Core Register    
        B4    0x02620140    Core Register    
        B5    0x20B00000    Core Register    
        B6    0x20B00FAC    Core Register    
        B7    0x21800004    Core Register    
        B8    0x80000000    Core Register    
        B9    0x21800004    Core Register    
        B10    0x02320018    Core Register    
        B11    0x0262003C    Core Register    
        B12    0x02310100    Core Register    
        B13    0x0000006A    Core Register    
        B14    0x00800E3C    Core Register    
        B15    0x0087FFA0    Core Register    
        B16    0x0016E35F    Core Register    
        B17    0x0087319C    Core Register    
        B18    0x00000181    Core Register    
        B19    0x0000000E    Core Register    
        B20    0x00000000    Core Register    
        B21    0x3000B000    Core Register    
        B22    0x22000008    Core Register    
        B23    0x12280110    Core Register    
        B24    0x01000423    Core Register    
        B25    0x05044684    Core Register    
        B26    0x38EA5601    Core Register    
        B27    0x04031000    Core Register    
        B28    0xC0AC0000    Core Register    
        B29    0x800A0103    Core Register    
        B30    0x0081D5CC    Core Register    
        B31    0x00000031    Core Register    
        AMR    0x00000000    Core Register: Addressing mode register    
            _RESV    0x0    Reserved    
            BK1    0x0    Block size 1    
            BK0    0x0    Block size 0    
            B7MODE    0x0 - LINEAR    B7 mode    
            B6MODE    0x0 - LINEAR    B6 mode    
            B5MODE    0x0 - LINEAR    B5 mode    
            B4MODE    0x0 - LINEAR    B4 mode    
            A7MODE    0x0 - LINEAR    A7 mode    
            A6MODE    0x0 - LINEAR    A6 mode    
            A5MODE    0x0 - LINEAR    A5 mode    
            A4MODE    0x0 - LINEAR    A4 mode    
        CSR    0x15000103    Core Register: Control status register    
            CPU_ID    0x15    CPU ID     
            REV_ID    0x00    Revision ID    
            PWRD    0x0    Control power-down modes    
            SAT    0x0 - NONSATURATE    Saturate     
            EN    0x1 - LITTLE    Endianness    
            PCC    0x0    Program Cache control mode    
            DCC    0x0    Data Cache control mode    
            PGIE    0x1    Previous GIE    
            GIE    0x1 - ENABLE    Global interrupt enable     
        IFR    0x00000000    Core Register: Interrupt Flag Register    
            _RESV    ****************    Reserved    
            IF15    0x0    Interrupt flag 15    
            IF14    0x0    Interrupt flag 14    
            IF13    0x0    Interrupt flag 13    
            IF12    0x0    Interrupt flag 12    
            IF11    0x0    Interrupt flag 11    
            IF10    0x0    Interrupt flag 10    
            IF9    0x0    Interrupt flag 9    
            IF8    0x0    Interrupt flag 8    
            IF7    0x0    Interrupt flag 7    
            IF6    0x0    Interrupt flag 6    
            IF5    0x0    Interrupt flag 5    
            IF4    0x0    Interrupt flag 4    
            _RESV    **    Reserved    
            NMIF    0x0    Non maskable Interrupt flag    
            _RESV    *    Reserved    
        ISR    0x00000000    Core Register: Interrupt Set Register    
            _RESV    0x0000    Reserved    
            IS15    0x0    Interrupt 15 Set    
            IS14    0x0    Interrupt 14 Set    
            IS13    0x0    Interrupt 15 Set    
            IS12    0x0    Interrupt 14 Set    
            IS11    0x0    Interrupt 15 Set    
            IS10    0x0    Interrupt 14 Set    
            IS9    0x0    Interrupt 15 Set    
            IS8    0x0    Interrupt 14 Set    
            IS7    0x0    Interrupt 15 Set    
            IS6    0x0    Interrupt 14 Set    
            IS5    0x0    Interrupt 15 Set    
            IS4    0x0    Interrupt 15 Set    
            _RESV    ****    Reserved    
        ICR    0x00000000    Core Register: Interrupt clear Register    
            _RESV    0x0000    Reserved    
            IC15    0x0    Interrupt 15 Clear    
            IC14    0x0    Interrupt 14 Clear    
            IC13    0x0    Interrupt 15 Clear    
            IC12    0x0    Interrupt 14 Clear    
            IC11    0x0    Interrupt 15 Clear    
            IC10    0x0    Interrupt 14 Clear    
            IC9    0x0    Interrupt 15 Clear    
            IC8    0x0    Interrupt 14 Clear    
            IC7    0x0    Interrupt 15 Clear    
            IC6    0x0    Interrupt 14 Clear    
            IC5    0x0    Interrupt 15 Clear    
            IC4    0x0    Interrupt 14 Clear    
            _RESV    ****    Reserved    
        IER    0x000003F3    Core Register: Interrupt enable Register    
            _RESV    ****************    Reserved    
            IE15    0x0 - DISABLE    Interrupt enable 15    
            IE14    0x0 - DISABLE    Interrupt enable 14    
            IE13    0x0 - DISABLE    Interrupt enable 13    
            IE12    0x0 - DISABLE    Interrupt enable 12    
            IE11    0x0 - DISABLE    Interrupt enable 11    
            IE10    0x0 - DISABLE    Interrupt enable 10    
            IE09    0x1 - ENABLE    Interrupt enable 9    
            IE08    0x1 - ENABLE    Interrupt enable 8    
            IE07    0x1 - ENABLE    Interrupt enable 7    
            IE06    0x1 - ENABLE    Interrupt enable 6    
            IE05    0x1 - ENABLE    Interrupt enable 5    
            IE04    0x1 - ENABLE    Interrupt enable 4    
            _RESV    **    Reserved    
            NMI    0x1    Non maskable interrupt    
            Reserved    *    
        ISTP    0x20B0FC00    Core Register: Interrupt service table pointer    
            ISTB    0x82C3F    Interrupt Service table base address    
            HPEINT    0x0    Specific interrupt occurred    
            _RESV    0x0    Reserved    
        IRP    0x20B01274    Core Register: Interrupt return pointer    
        NRP    0x00000000    Core Register: Non maskable interrupt    
        ERP    0x00000000    Core Register: Exception return pointer    
        TSCL    0x00000000    Core Register: Low half of 64-bit timestamp    
        TSCH    0x00000000    Core Register: High half of 64-bit timestamp    
        ARP    0x00000000    Core Register: Analysis return pointer    
        ILC    0x00000000    Core Register: Inner loop SPL buffer count    
        RILC    0x00000000    Core Register: Reload Inner loop SPL buffer count    
        PCE1    0x20B01270    Core Register: Program counter E1 phase    
        DNUM    0x00000000    Core Register: DSP Number    
            _RESV    0x000000    Reserved    
            DSPNUM    0x00    
        FADCR    0x00000000    Core Register: Floating Point Register    
        FAUCR    0x00000000    Core Register: Floating Point Register    
        FMCR    0x00000000    Core Register: Floating Point Register    
        SSR    0x00000000    Core Register: Saturation status register    
            RESV    0x000000    Reserved    
            M2    0x0    Saturation in M2 Unit    
            M1    0x0    Saturation in M1 Unit    
            S2    0x0    Saturation in S2 Unit    
            S1    0x0    Saturation in S1 Unit    
            L2    0x0    Saturation in L2 Unit    
            L1    0x0    Saturation in L1 Unit    
        GPLYA    0x00000000    Core Register: GMPY polynomial for A-side    
        GPLYB    0x00000000    Core Register: GMPY polynomial for B-side    
        GFPGFR    0x0700001D    Core Register: Galois field multiply control register    
            _RESV    0x0    Reserved    
            SIZE    0x7    Size    
            _RESV    0x0000    Reserved    
            POLY    0x1D    Polynomial    
        DIER    0x00000000    Core Register: Debug interrupt enable register    
        TSR    0x00000001    Core Register: Task state register    
            _RESV    0x0000    Reserved    
            IB    0x0 - UNBLOCKED    Interrupts blocked    
            SPLX    0x0 - NOTEXEC    SPLOOP Executing     
            _RESV    0x0    Reserved    
            EXC    0x0 - NOTEXEC    Execption Processing    
            INT    0x0 - NOTEXEC    Interrupt Processing    
            _RESV    0x0    Reserved    
            CXM    0x0 - SUPERVISOR    Current Execution Mode    
            _RESV    0x0    Reserved    
            DBGM    0x0 - EMU_ENABLE    Emulator debug mask    
            XEN    0x0 - DISABLE    Maskable exception enable    
            GEE    0x0 - DISABLE    Globale exception enable    
            SGIE    0x0    Saved global interrupt enable    
            GIE    0x1 - ENABLE    Global interrupt enable    
        ITSR    0x00000001    Core Register: Interrupt task state register    
            _RESV    0x0000    Reserved    
            IB    0x0 - UNBLOCKED    Interrupts blocked    
            SPLX    0x0 - NOTEXEC    SPLOOP Executing     
            _RESV    0x0    Reserved    
            EXC    0x0 - NOTEXEC    Execption Processing    
            INT    0x0 - NOTEXEC    Interrupt Processing    
            _RESV    0x0    Reserved    
            CXM    0x0 - SUPERVISOR    Current Execution Mode    
            _RESV    0x0    Reserved    
            DBGM    0x0 - EMU_ENABLE    Emulator debug mask    
            XEN    0x0 - DISABLE    Maskable exception enable    
            GEE    0x0 - DISABLE    Globale exception enable    
            SGIE    0x0    Saved global interrupt enable    
            GIE    0x1 - ENABLE    Global interrupt enable    
        NTSR    0x00010000    Core Register: Non maskable TSR snapshot    
            _RESV    0x0001    Reserved    
            IB    0x0 - UNBLOCKED    Interrupts blocked    
            SPLX    0x0 - NOTEXEC    SPLOOP Executing     
            _RESV    0x0    Reserved    
            EXC    0x0 - NOTEXEC    Execption Processing    
            INT    0x0 - NOTEXEC    Interrupt Processing    
            _RESV    0x0    Reserved    
            CXM    0x0 - SUPERVISOR    Current Execution Mode    
            _RESV    0x0    Reserved    
            DBGM    0x0 - EMU_ENABLE    Emulator debug mask    
            XEN    0x0 - DISABLE    Maskable exception enable    
            GEE    0x0 - DISABLE    Globale exception enable    
            SGIE    0x0    Saved global interrupt enable    
            GIE    0x0 - DISABLE    Global interrupt enable    
        ETSR    0x00010000    Core Register: Exception TSR snapshot    
            _RESV    0x0001    Reserved    
            IB    0x0    Interrupts blocked    
            SPLX    0x0    SPLOOP Executing     
            _RESV    0x0    Reserved    
            EXC    0x0    Execption Processing    
            INT    0x0    Interrupt Processing    
            _RESV    0x0    Reserved    
            CXM    0x0    Current Execution Mode    
            _RESV    0x0    Reserved    
            DBGM    0x0    Emulator debug mask    
            XEN    0x0    Maskable exception enable    
            GEE    0x0    Globale exception enable    
            SGIE    0x0    Saved global interrupt enable    
            GIE    0x0    Global interrupt enable    
        EFR    0x00000000    Core Register: Exception Flag Register    
            NXF    0x0    NMI Exception flag    
            EXF    0x0    EXCEP Exception flag    
            _RESV    0x0000000    Reserved    
            IXF    0x0    Internal Exception flag    
            OXF    0x0    OSSR Exception flag    
        ECR    0x00000000    Core Register: Exception clear register    
            NXC    0x0    NMI Exception Clear    
            EXC    0x0    EXCEP Exception Clear    
            _RESV    0x0000000    Reserved    
            IXC    0x0    Internal Exception Clear    
            OXC    0x0    OSSR Exception Clear    
        IERR    0x00000000    Core Register: Internal exception cause register    
    RegisterPairs    RegisterPairs    
        A1_A0    0x0000000100000001    Core Register    
        A3_A2    0x0100000001000000    Core Register    
        A5_A4    0x2000000001845044    Core Register    
        A7_A6    0x0000000000000018    Core Register    
        A9_A8    0x20B09A8021800004    Core Register    
        A11_A10    0x0087FFFC000003F0    Core Register    
        A13_A12    0x0087370002320010    Core Register    
        A15_A14    0x008734A800873680    Core Register    
        A17_A16    0x002625A000000000    Core Register    
        A19_A18    0x000000000002625A    Core Register    
        A21_A20    0x00EE6B2800000000    Core Register    
        A23_A22    0x0040202C00873680    Core Register    
        A25_A24    0x0081D5CC00000010    Core Register    
        A27_A26    0x000000010081D5CC    Core Register    
        A29_A28    0x0081EFCC00000000    Core Register    
        A31_A30    0x0000000000000001    Core Register    
        B1_B0    0x2000000121000001    Core Register    
        B3_B2    0x20B0126400000000    Core Register    
        B5_B4    0x20B0000002620140    Core Register    
        B7_B6    0x2180000420B00FAC    Core Register    
        B9_B8    0x2180000480000000    Core Register    
        B11_B10    0x0262003C02320018    Core Register    
        B13_B12    0x0000006A02310100    Core Register    
        B15_B14    0x0087FFA000800E3C    Core Register    
        B17_B16    0x0087319C0016E35F    Core Register    
        B19_B18    0x0000000E00000181    Core Register    
        B21_B20    0x3000B00000000000    Core Register    
        B23_B22    0x1228011022000008    Core Register    
        B25_B24    0x0504468401000423    Core Register    
        B27_B26    0x0403100038EA5601    Core Register    
        B29_B28    0x800A0103C0AC0000    Core Register    
        B31_B30    0x000000310081D5CC    Core Register    

    The config space registers read out:

    dumping regs
    ------------
    read register 0x00000000, value 0x4e301100
    read register 0x00000004, value 0x00000005
    read register 0x00000008, value 0x00000000
    read register 0x0000000c, value 0x00000000
    read register 0x00000010, value 0x00000000
    read register 0x00000014, value 0x00010000
    read register 0x00000020, value 0x00000000
    read register 0x00000024, value 0x00000000
    read register 0x00000028, value 0x00000000
    read register 0x00000030, value 0x00000000
    read register 0x00000034, value 0x00000000
    read register 0x00000038, value 0x00000000
    read register 0x0000003c, value 0x00000000
    read register 0x00000050, value 0x00000000
    read register 0x00000054, value 0x00000000
    read register 0x00000064, value 0x00000000
    read register 0x00000068, value 0x00000000
    read register 0x0000006c, value 0x00000000
    read register 0x00000070, value 0x00000000
    read register 0x00000074, value 0x00000000
    read register 0x00000078, value 0x00000000
    read register 0x0000007c, value 0x00000000
    read register 0x00000100, value 0x00000000
    read register 0x00000104, value 0x00000000
    read register 0x00000108, value 0x00000001
    read register 0x0000010c, value 0x00000001
    read register 0x00000110, value 0x00000000
    read register 0x00000114, value 0x00000000
    read register 0x00000118, value 0x00000000
    read register 0x0000011c, value 0x00000000
    read register 0x00000120, value 0x00000000
    read register 0x00000124, value 0x00000000
    read register 0x00000128, value 0x00000000
    read register 0x0000012c, value 0x00000000
    read register 0x00000130, value 0x00000000
    read register 0x00000134, value 0x00000000
    read register 0x00000138, value 0x00000000
    read register 0x0000013c, value 0x00000000
    read register 0x00000140, value 0x00000000
    read register 0x00000144, value 0x00000000
    read register 0x00000148, value 0x00000000
    read register 0x0000014c, value 0x00000000
    read register 0x00000150, value 0x00000000
    read register 0x00000154, value 0x00000000
    read register 0x00000158, value 0x00000000
    read register 0x0000015c, value 0x00000000
    read register 0x00000160, value 0x00000000
    read register 0x00000164, value 0x00000000
    read register 0x00000168, value 0x00000000
    read register 0x0000016c, value 0x00000000
    read register 0x00000170, value 0x00000008
    read register 0x00000174, value 0x00000000
    read register 0x00000178, value 0x00000000
    read register 0x0000017c, value 0x00000000
    read register 0x00000180, value 0x00000000
    read register 0x00000184, value 0x00000000
    read register 0x00000188, value 0x00000001
    read register 0x0000018c, value 0x00000001
    read register 0x00000190, value 0x00000000
    read register 0x00000194, value 0x00000000
    read register 0x00000198, value 0x00000001
    read register 0x0000019c, value 0x00000001
    read register 0x000001a0, value 0x00000000
    read register 0x000001a4, value 0x00000000
    read register 0x000001a8, value 0x00000001
    read register 0x000001ac, value 0x00000001
    read register 0x000001b0, value 0x00000000
    read register 0x000001b4, value 0x00000000
    read register 0x000001b8, value 0x00000001
    read register 0x000001bc, value 0x00000001
    read register 0x000001c0, value 0x00000000
    read register 0x000001c4, value 0x00000000
    read register 0x000001c8, value 0x00000000
    read register 0x000001cc, value 0x00000000
    read register 0x000001d0, value 0x00000000
    read register 0x000001d4, value 0x00000000
    read register 0x000001d8, value 0x00000000
    read register 0x000001dc, value 0x00000000
    read register 0x00000300, value 0x00000001
    read register 0x00000304, value 0xca400000
    read register 0x00000308, value 0x00000000
    read register 0x0000030c, value 0x10800000
    read register 0x00000310, value 0x00000002
    read register 0x00000314, value 0x11800000
    read register 0x00000318, value 0x00000000
    read register 0x0000031c, value 0x00000000
    read register 0x00000320, value 0x00000003
    read register 0x00000324, value 0x12800000
    read register 0x00000328, value 0x00000000
    read register 0x0000032c, value 0x00000000
    read register 0x00000330, value 0x00000004
    read register 0x00000334, value 0x80000000
    read register 0x00000338, value 0x00000000
    read register 0x0000033c, value 0x00000000
    read register 0x00000380, value 0x00002110
    read register 0x00000384, value 0x00000000
    read register 0x00000388, value 0x00001333
    read register 0x00000390, value 0x000622a0
    read register 0x00000394, value 0x000222a0
    ------------

  • Gert,

    Based on the dump of PCIe registers, it looks like the MSI0 is enabled (MSI0_IRQ_ENABLE_SET (0x108)=1), but there is no MSI0 interrupt being triggered (MSI0_IRQ_STATUS_RAW (0x100) = 0). Instead, the MSI7 status register has some bit being set as MSI7_IRQ_STATUS_RAW (0x170) = 0x8. It may raise the question that if the MSI0 interrupt is really being triggered in the second time (after reset).

    I am not sure what the "SWAP(0xff00)" is doing in the following code section you mentioned before. Could you double check if the MSI0 is actually being triggered (write 0x0 to MSI_IRQ (0x54)) please?

        /* Now poke the legacy interrupt on the EP to have it break out of boot.
        Do it twice just to be sure */
        if (do_prints) printf("set registers... trigger INT\n");
        pRegister = (unsigned int *) ( ((unsigned int) p_mapped) + TI_MSI_IRQ);
        *pRegister = SWAP(0xff00); /*    This register is written to by the remote device. Writes initiated by an EP over PCIe link that target
                                        BAR0 of the RC land to this register if the offset matches. To generate MSI Interrupt 0, the EP should
                                        write 0x0000_0000 to this register. It will result in a pulse on bit zero triggering the MSI interrupt
                                        from PCIESS to the external processor. */
        if (do_prints) printf("set registers... trigger INT..DONE1\n");
        *pRegister = SWAP(0xff00);
        if (do_prints) printf("set registers... trigger INT..DONE2\n");

    Sincerely,

    Steven

  • Hi Steven,

    I double-checked and write 0x00000000 twice to MSI_IRQ (0x54). The same outcome.

    Br,

    Gert.

  • Hi Gert, sorry for the delay, I've been out of office, working on other stuff, etc.

    I am loading over PCIe.

    We use R1.0 Silicon C6678 on EVM board, with the PLL workaround. So the C6678 first loads the PLL workaround from I2C, then configures PCIe and waits for the Root Complex to download software and set Boot Magic Address.

    The version of the PLL workaround bootloader that we use does not expect an MSI interrupt. It just sits in a loop reading the boot magic address until it is non-zero.

    We also do the same thing on some boards we built ourself (some with R1.0 silicon, some with R2.0), but in both cases using the PLL workaround first loaded from I2C then load over PCIe with Boot Magic Address set by RC.

    We are just starting to experiment with R2.0 silicon without the PLL workaround (because not needed with R2.0), direct boot purely from the ROM boot loader over PCIe.

    In that case, I notice the behavior is a bit different. The RC host has to write the Boot Magic Address, then send an MSI interrupt (data 0 to DSP address 0x21800054).

    I did notice that if the MSI is sent while Boot Magic Adress is still zero, the C6678 seems to lock up and ignore any later MSI that is sent after setting boot magic address.

    So it's important to set magic address on Core 0 (and read it back to flush the write buffers) before sending any MSI.

    That's as far as I've got, and am working on something more urgent right now.

    Regards, Jonathan

  • Thanks Jonathan.

    We opened a support ticket for this.

    Best regards,

    Gert.