Hi TI experts,
This is my first time to experience OMAPL138. There are several issues that I really appreciate for your advices.
Even though I purchased OMAPL138 EVMs but I only want to experience C6748 SOM-M1 only to develop our camera device using neither external RAM nor OS.
Our design at this step is simply enough to require only VPIF and USB OTG. To be more specific, C6748 will interface with a image sensor and stream images back to PC through USB OTG.Due to cost stringency, we would like to utilize internal RAMs for program memory and programmable ROM for boot image.
Because this is my first approach to TI DSP, there are many questions that I need to search for the answers before we can officially start the project. Your expertise will help us to make a quick grasp on the technology to accelerate our development.
1. Are internal RAMs enough for StarterWare to work? How can we make it to work with internal RAM only?
2. Can we mask our final image into internal ROM and let DSP boot directly from ROM without boot loader?
3. Can we disable external RAM in the EVMs and direct it to use internal RAMs? In other words, what should we do with EVMs to start the development of our device (without ext RAM and OS).
4. Is there any existing UVC device firmware code for C6000? If there is none, a similar sample for streaming video through USB is a great help for us.
5. Is there any development manual that helps us to program with internal RAMs and without using OS?
6. Does DSP/BIOS help to reduce the development labor in our case? How much is its size when residing in the boot storage?
Thank you very much for your supports,
Best regards,
Tuyen Nguyen