This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 SPI portnumber PLL



Hi all,

    I am trying to boot from SPI Nor Flash on custom board based on C6678. The device silicon revision number is 1.0.

I learned that port number indicates where to boot from and the port number of I2C is 0.

1. Then which is the port number of SPI ?

    Is there any document which mentions the allocation of port number?

2. I don't know wether the bootloader code contains the PLL initialization or not.

    So do i need to program PLL initialization code and set main PLL in bypass mode in my own application?

Please help me.

Thanks.

Nuoxi 

  • Nuoxi, I thinkyour question on PLL initialization was addressed by Arun in the last post here: http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/101820.aspx

    I also saw that you posted questions for SPI port num in this thread: http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/115298.aspx?PageIndex=6

    Please try to limit the number of posts on the same topic. That way it is easier for us to sort through various posts and respond as quickly as possible. Thanks.