Hi.
I have evaluation module from Mistral with DDR3 2x512M. I try to use psp 04.01.00.07. Now i can run Matrix Application, but multimedia demos and 3D graphics don't run. When i click "run", the following message apeares on the console:
VPSS_GRPX : please open fb1 node first.
Assertion at Line no: 445 in /build/a0868651/toolchains/syslink_2_00_04_83/packa
ges/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Li
nux/SharedRegionDrv.c: (heapHandle != NULL) : failed
VPSS_GRPX : please open fb1 node first.
I use prebuild syslink.ko from psp.
Can Matrix application work with psp 04.01.00.07?