This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Getting started with Ezsdk

  Respected Sir/Madam,

  i have just started learning ezsdk and soon will start working on it but i have some questions:

1.  Is it necessary to have SD card for working with ezsdk or can we also just use jtag for flashing NAND and start working, if yes how can we do that?

2. How can we integrate ccs with ezsdk so that the buitin libraries that come with ezsdk can be used in ccs?

3. As far as i come to know that first step for working with  ezsdk is to load linux kernel to target processor.Why is it necessary to load linux kernel to the target processor for start development using ezsdk?

I am using DM8148(Centaurus board) and right now i don't have SD card or MMC. can u plz throw some light over these question? I am much confuse at this moment.