Other Parts Discussed in Thread: TVP5158, TVP5146
Anshuman,
I'm reposting this. I have questions regarding the TVP5158 driver release that was announced in June 2011:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/t/118704.aspx.
It appears that the TVP5158 driver requires a significant level of effort to integrate into a udworks DM36x reference DVR. See the following forum threads:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/t/162211.aspx
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/t/166892.aspx
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/t/160657.aspx
Because I was under the impression that this 5158 driver release was developed & validated on the DM36x DVR platform - the release notes state that the release 00.02.00 was validated on a DM365 DVR - these issues come as a surprise and concern to me. I've been working on the 5158 driver for several weeks w/a Leopardboard 368, and I'm not seeing that the current driver fits at all well on that platform either.
At this point, it's clear that I need to better understand the current state of development on the 5158 driver. I've been using the DM365_DVR_DVSDK3_00.02.00.00.zip release package that you announced in June 2011, on the 4.02 DVSDK for the DM368. In the TVP5158 driver announcement, you state that this driver is for the DM36x, based on DVSDK 3.x and kernel 2.6.32, and again, the release notes state that the release was validated on a DM365 DVR.
- On what specific DM36x platform did TI develop and validate this driver release?
- This driver release from last summer has missing components, such as audio support, and is filled w/personalizations, including multiple references to user 'deepu' and his/her home directory. The driver comes across as incomplete and a work-in-progress. Are there plans and a timeline for an updated release?
regards,
gifford scott