I am designing the power supply to an AM3352. I am not intending to use the RTC on the AM3352.
Question 1: For disabling the RTC I follow the instructions in the "AM335x Schematic Checklist" under "RTC internal oscillator is not used...", correct?
Question2: While using an AM335X with a disabled RTC do I follow Figure 4-5 "Power-Supply Sequencing with RTC Feature Disabled" on page 95 of the datasheet? I am assuming I do, but what if I use 1.8V and 3.3V I/O? There is no specific mention of the mixed voltage I/O where there is in the previous Power Up Sequence figures such as Figure 4-2.
Thanks.