This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

1st IDR cause unstable



Hi

I have a problem about the H.264 decode. I have the h.264 decoder version (1.10.04) which is coming with the dvsdk_3_10_00_19. It works but it has some defect. Here is the description.

I played the H.264 elementary stream with the 720p. The first frame is the IDR slice and it can be decoded by the codecs. However, the output of the frame is full of blocks and unstable. I don't receive any error from the codecs. The worst thing is this frame affect the rest of the stream. The playback will become unstable (like shutter and color fadding).

If I skip the first IDR slice and play the rest of the stream. The first few frames will be shutter and grey in color because it doesn't have the IDR slice. It will become normal when the next IDR slice is received. Afterward, everything will become normal and smooth.

Is there any insight about this ? Is it related with codec?

Best Regards,

Philip Lee