This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM1808 vs AM335x Power Comparision

Other Parts Discussed in Thread: AM1808

TI,

I am looking for a static image power comparision between the AM335x and AM1808.  I see Am335x has this scenario spelled out.  I did not see the same information for the AM1808 is there a comparision from AM1808 power summary:

No OS : Static Image Display

Software : Bare metal code
Use Case : Display a static image on the LCD panel
OPP : OPP100 (ARM 550 MHz, DDR 200 MHz, L3 200 MHz, L4 100 MHz)

Power Supply Nominal Rating Jumper Shunt [Ohm] Voltage Drop [mV] Voltage [V] Current [mA] Power [mW]
VDD_CORE 1.1V +/-4% N/A 0.05 9.32 1.097 186.40 204.48
VDD_MPU 1.1V – 1.3V +/-4% N/A 0.05 5.99 1.104 119.89 132.36
VDDS_RTC 1.8V +/-5% J35 2 0.62 1.826 0.31 0.57
VDDS_DDR 1.8V +/-5% / 1.5V +/-5% J20 0.24 4.96 1.800 20.67 37.19
VDDS 1.8V +/-5% J21 0.24 0.10 1.796 0.41 0.73
VDDS_SRAM_CORE_BG 1.8V +/-5% J23 2 2.49 1.813 1.25 2.26
VDDS_SRAM_MPU_BB 1.8V +/-5% J25 2 2.48 1.813 1.24 2.25
VDDS_PLL_DDR 1.8V +/-5% J33 2 2.05 1.813 1.02 1.86
VDDS_PLL_CORE_LCD 1.8V +/-5% J24 2 13.71 1.799 6.85 12.33
VDDS_PLL_MPU 1.8V +/-5% J22 2 3.37 1.809 1.69 3.05
VDDS_OSC 1.8V +/-5% J29 2 1.34 1.812 0.67 1.22
VDDA1P8V_USB0/1 1.8V +/-5% J28 1 3.25 1.818 3.25 5.91
VDDA3P3V_USB0/1 3.3V +/-5% J31 2 0.06 3.316 0.03 0.09
VDDA_ADC 1.8V +/-5% J27 1 0.45 1.816 0.45 0.82
VDDSHV1 1.8 / 3.3 V +/-5% J26 0.24 0.01 3.326 0.02 0.07
VDDSHV2 1.8 / 3.3 V +/-5% J38 0.24 0.03 3.292 0.11 0.37
VDDSHV3 1.8 / 3.3 V +/-5% J39 0.24 0.01 3.327 0.05 0.18
VDDSHV4 1.8 / 3.3 V +/-5% J30 0.24 0.00 3.292 0.01 0.04
VDDSHV5 1.8 / 3.3 V +/-5% J32 0.24 0.01 3.326 0.04 0.12
VDDSHV6 1.8 / 3.3 V +/-5% J34 0.24 0.97 3.325 4.04 13.44
            Total 419.36

 

-Jason

  • Jason

    For AM18xx, such a use-case has not been profiled.

    It would be best to get an "estimate" of the equivalent use-case using the power estimation spreadsheet for AM18xx

    http://processors.wiki.ti.com/index.php/AM18x_Power_Consumption_Summary

    Regards

    Mukul