Other Parts Discussed in Thread: OMAPL138
Hi,
Q1: What is Texas Instruments design recommendations on the OMAPL138 for USB0_VBUS connected to a host (PC), when the OMAPL138 is powered off?
Q2: What is Texas Instruments design recommendations on the OMAPL138 for USB0_DM, USB0_DP, connected to a host (PC), when the OMAPL138 is powered off?
If the OMAP USB0_BUS can NOT be connected to a HOST while powered off, why is this not listed or described in the datasheets.
Please clarify in detail.
Background:
One can measure a voltage around 350mV on the DVDD3318/ USB0_VDDA33 power rails, when VBUS is +5V and present.
This thread indicate that the use-case is unsupported: http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/96557.aspx
/Magnus