This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359 Linux Kernel 3.2 Power Management

I am currently using the Angstrom distro with the 3.2.11+ kernel on a beagle bone and have included cpuidle parameters and pm_sleep in the defconfig.  I get the /sys populated with the cpuidle parameters but there is no sleep_while_idle parameter in sys/kernel/debug/pm_debug/  to enable/disable cpuidle.  Is this part of the PSP currently working on kernel 3.2 or is there some missing configuration item in the angstrom release.  As a not i tried this on the ti kernel as well and it showed the same behavior.  Any help would be greatly appreciated as i need to get power management numbers for the project i am working.

Thanks

Ed