I have DSP application which run on DM642 processor. That application is developed in CCS 3.3 environment and linked to the library which I have no sources, so I can't recompile it. My question is whether I can recompile and run the same application on the newer DSP such as DM6441, DM6443, DM6446 or DM6437?
In other words whether these DSP are backward compatible and will support my old library?
Thanks