This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How can we configure VDD1 in TPS65930 to 1.35v with Smart Reflex Mode Enabled?

We tried the following thing but dint worked.

SmartReflex control of the VDD1 and VDD2 regulators can be enabled by setting the DCDC_GLOBAL_CFG[3] SMARTREFLEX_ENABLE bit to 1. To perform VDD1 voltage control through the SmartReflex interface, the device provides the VDD1_SR_CONTROL register. The VDD1_SR_CONTROL MODE bit field can be set to 0 to put VDD1 in an ACTIVE state; setting the field to1 moves VDD1 to a SLEEP state. VDD1 output voltage can be programmed by setting the VDD1_SR_CONTROL VSEL bit field. VDD1 output voltage is given by VSEL*12.5 mV + 600 mV.

 Can anybody let us know if any additional settings is required?