Hi,
i would like to do some testing using AM335x EVM and Micrel KSZ9021RL eval board before i design my custom board.
in hardware connection, can i use RGMII2 on the AM335x EVM? the Expansion Connector - EXP3:
Can we configure this Header to RGMII2 interface as below? so that i can use these pin connect to Micrel ethernet eval board.
pin2: AM335X_GPMC_A0 (RGMII2_TCTL)
pin4: SDIC_GPMC_A1 (RGMII2_RCTL)
pin6: SDIC_GPMC_A2 (RGMII2_TD3)
pin8: SDIC_GPMC_A3 (RGMII2_TD2)
pin10: AM335X_GPMC_A4 (RGMII2_TD1)
pin12: AM335X_GPMC_A5 (RGMII2_TD0)
pin16: AM335X_GPMC_A6 (RGMII2_TCLK)
pin18: AM335X_GPMC_A7 (RGMII2_RCLK)
pin22: AM335X_GPMC_A8 (RGMII2_RD3)
pin24: AM335X_GPMC_A9 (RGMII2_RD2)
pin26: AM335X_GPMC_A10 (RGMII2_RD1)
pin28: AM335X_GPMC_A11 (RGMII2_RD0)
Thanks and Regards
Keldy