Other Parts Discussed in Thread: OMAP-L138, TMS320C6748
We've successfully finished a project where we utilized C6747 processor. Our new project has a C6748 and I'd like to get a little help on this.
We have many new interfaces in the new project. The most important ones are SPI interface for boot flash and RMII ethernet. We're planning to use DSP/BIOS but you suggest Linux is easier that's ok to us (we've used Linux on FPGA softcores).
The first question is that is there a free bootloader code for the SPI interface? And how about code for TCP/IP ethernet stack?
We have used McASP in analog IF but going to use McBSP in our new project. Any suggestions what to read first (when going from McASP->McBSP)?
And finally we'd like to test as much as possible on a evaluation board before our protos come out. Do you think SOMC6748-10-1602AHCR could be a good choice to us / is there any better ones?
Many thanks! :)