This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 power down sequence requirements



Hello,

I have seen all of the earlier posts regarding the power-down sequence, including this one: http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/146484.aspx. However, I am not satisfied with the answer.

We have a design which, like the eval board, uses an FPGA to control the power sequencing for the DSP. The reset protocol used on our design is the same as that is used on the eval board, and does not include any power-down sequencing. Oviously, it is not possible to sequence off DSP power rails when the power inputs are removed, as with a hard shut-down. And power cannot be sequenced off properly, as per the datasheet, if a POR is asserted due to a loss of any of the rails other than that which should be removed first according to the sequencing requirements. So the only plausible scenario for implementing a power-down sequence as it is defined in the datasheet is if a power-on reset is asserted for reasons other than a power failure. So my question is: How important is it really to employ a power-down sequence for the single situation that would allow it, when all other situations make it impossible?

Thanks.

-Courtney

  • Courtney,

    I think you've pointed out that there are really only two scenarios, power failure and shutting down the power of the device.  This thread discusses this http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/140558.aspx.  I assume you want to shut down the device at some point and simply pulling the power as would be the case for a power failure is not the way to do it.  The guideline is for the normal powering down of the device which may be necessary from time to time.  Some people may even power specific boards/devices down during low load conditions.  These would go through many power down sequences over it's life and these would be most at risk if a power down sequence was not implemented.

    Best Regards,
    Chad