Hi,all ,I tried to use core 0 to sending a ipc interupt to core 1,then core 1 send a ipc interupt back to core 0 after receiving the ipc interrupt from core 0 .i use CSL_IPC_genGEMInterrupt(1,0) ( for core 0) and CSL_IPC_IsGEMInterrupt Ackset(1,0) (for core 1)to do this ,and I found that if I do DDR_init() , core 1 can’t receive the ipc interrupt from core 0 , I also tried to import evmc6678l.gel to do all the initional instead of using DDR_init(),which happened too.i also tried not to do DDR_init() before sending a ipc interrupt ,and I found the core 1 can receive the interrupt from core 0 . I don’t know why this happened , could you give me some suggestions?
And can I get a ipc hardware datasheet since I can’t find it in the website?