Other Parts Discussed in Thread: OMAPL138
Dear I have problem during compiling starterware application via cygwin-gcc.

Can you help me ?
Sergio D'Orazio.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAPL138
Dear I have problem during compiling starterware application via cygwin-gcc.

Can you help me ?
Sergio D'Orazio.
Probably you cannot read the image.... the error is:
~/ti/OMAPL138_StarterWare_1_10_03_03/build/armv5/gcc/omapl138/evmOMAPL138/usb_dev_msc
$ make all
make TARGET_MODE=debug lib
make[1]: Entering directory `C:/cygwin/home/T0102950/ti/OMAPL138_StarterWare_1_10_03_03/build/armv5/gcc/omapl138/evmOMAPL138/usb_dev_msc'
C:/cygwin/tmp/make684-1.sh: line 1: syntax error near unexpected token `$'\\\r''
C:/cygwin/tmp/make684-1.sh: line 1: `for i in ../../../../../..//build/armv5/gcc/omapl138/drivers ../../../../../..//build/armv5/gcc/omapl138/evmOMAPL138/platform ../../../../../..//buil5/gcc/omapl138/system_config ../../../../../..//build/armv5/gcc/utils ../../../../../..//build/armv5/gcc/grlib ../../../../../..//build/armv5/gcc/omapl138/usblib; ' \
make[1]: *** [lib] Error 2
make[1]: Leaving directory `C:/cygwin/home/T0102950/ti/OMAPL138_StarterWare_1_10_03_03/build/armv5/gcc/omapl138/evmOMAPL138/usb_dev_msc'
make: *** [debug] Error 2
T0102950@IT30D10034
~/ti/OMAPL138_StarterWare_1_10_03_03/build/armv5/gcc/omapl138/evmOMAPL138/usb_dev_msc
By.
Sergio D'Orazio.
Sergio,
What shell are you using in Cygwin? The makefiles were developed for use with bash, so it's possible that some modification may be necessary if you're using a different shell. You can quickly check your shell by running ps in the Cygwin terminal. You should see something like this if you're using bash:
PID PPID PGID WINPID TTY UID STIME COMMAND
10440 6668 10440 10668 pty0 452561 17:27:59 /usr/bin/ps
6668 6832 6668 3484 pty0 452561 Mar 14 /usr/bin/bash
6832 1 6832 6832 ? 452561 Mar 14 /usr/bin/mintty
Hope this helps.