Other Parts Discussed in Thread: TMDXEVM3358, AM3352
Hello
I have a customer evaluating our AM335x family using our TMDXEVM3358 and have a few questions about the Linux SDK provided, which hopefully you can help me with.
1. Is it possible to alter the CPU speed to check the operation of the various speed grades available.
I know there is often a "cpu-freq-set" function but can you confirm this or something similar is included in the SDK and where it is located
There doesn't appear to be anything in the Matrix GUI demo to do this.
2. They wish to evaluate the Graphics performance of the AM3352 (i.e. without the GPU) so can you tell me what graphics demo's are available that don't use the
SGX530 GPU.
Sorry if these are a little basic but I don't have an EVM to look myself.
Many Thanks
Bob Bacon