Other Parts Discussed in Thread: DM3730, OMAP3530
Hi everybody
I am using CCS Version: 5.1.1.00031, DM3730, XDS100v2 on windows 7 32 bit
On my C64x+ side , i was trying to run SYS/BIOS examples, there i was getting error like ../../gptimer/Timer.c could not locate.
then i locate that file as it was asking. then i load my code again , but it is going in automatic running and from Timer.c I can see Program counter as below, that means code is going on waiting state at this point ..
In short I am not able to run even this example, i have worked on SYS/BIOS earlier on OMAP3530, but didn't faced this kind of situation.
Note: i guess SYS/BIOS project is missing Timer.c somewhere in there include files.
Does anybody have clue on this
With Regards
Nitin Mewada