This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM36x H264ENCCODER version.02.30.00.04 CVBR Bitrate condition

Hi all,

The above codec version i am getting error while setting runtime parameters with Error code 0xA006 which corresponds to CVBR Bitrate.

But as per the error codes it states that

0 < maxBitrate CVBR < max bitrate

and my bitrate condition satisfies the above. Older versions works fine with the above condition.

Please update us if any changes in the specification for the same version of codec. Also i don't see any document stating the same condition anr any change spec for the above.

I would appriciate to have the updated info on the same.