Hi,
I am developing an application on OMAP L138 EVM, using DSP/BIOS Link shared memory mechanism. The board supports 64MB of DDR2 memory.
For my application , I modified the 'read write' sample program. But now the CODE/DATA(DDR) space is not enough for fitting my DSP executable.
So I increased the DDR(CODE/DATA) space.
This was the default memory configuration of read write program.
RESET_VECTOR.base = 0xC3E00000 ;
RESET_VECTOR.len = 0x00000080;
DDR.base = 0xC3E00080 ;
DDR.len = 0xFFF80;
DSPLINKMEM.base = 0xC3F00000;
DSPLINKMEM.len = 0x30000;
POOLMEM.base = 0xC3F30000 ;
POOLMEM.len = 0xD0000 ;
In this configuration, from address 0xC3E00000 to 0xC4000000, is configured for DSP.
Since the 64MB DDR2 address range is from 0xC0000000 to 0xC4000000,
if I try to increase DDR memory, the memory configuration will go out of the bound 0xC4000000.
So I shifted the RESET_VECTOR address to 0xC3D00000, and increased the DDR memory.
But now I am getting error when running program.
In my UBOOT boot arg, the MEM parameter is set to 32M, then I think the remaining 32MB can be used by DSP .
ie memory region from 0xC2000000 to 0xC4000000 is accessible by DSP.
Then what is the problem of accessing memory location before the address 0xC3E00000.
I am attaching my new memory configurations files here.
/** ============================================================================ * @file CFG_OMAPL138GEM_SHMEM.c * * @path $(DSPLINK)/config/all/ * * @desc Defines the configuration information for DSP/BIOS LINK for the * OMAPL138 platform. * * @ver 1.65.01.05_eng * ============================================================================ * Copyright (C) 2002-2009, Texas Instruments Incorporated - * http://www.ti.com/ * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ============================================================================ */ /* ----------------------------------- DSP/BIOS LINK Headers */ #include <dsplink.h> #include <procdefs.h> #if defined (__cplusplus) EXTERN "C" { #endif /* defined (__cplusplus) */ /** ============================================================================ * DSPLINK MEMORY SECTION DIAGRAM * * |--------------[ 0xXXXXXX00 ]---------------------------------| * | | * | RESET VECTOR (0x80) | * | Last two nibbles must be zero | * | | * |-------------------------------------------------------------| * | | * | DSP CODE/DATA | * | DSP executable is loaded to this section | * | | * |=============================================================| * | | * | DSPLINK SHARED MEMORY0 | * | Shared control structure is loaded here | * | | * |-------------------------------------------------------------| * | | * | DSPLINK SHARED MEMORY1 | * | Shared control structure is loaded here | * | | * |-------------------------------------------------------------| * | | * | POOL Buffer Memory | * | Pool's buffers are created in this area | * | | * |-------------------------------------------------------------| * * ============================================================================ */ /** ============================================================================ * @name DRVHANDSHAKEPOLLCOUNT * * @desc POLL Count for Driver handshake. * ============================================================================ */ #define DRVHANDSHAKEPOLLCOUNT ((Uint32) -1u) /** ============================================================================ * @name RESETCTRLADDR * * @desc Indicates the start address of Reset Ctrl memory region. * last two nibbles must be zero i.e. align to 256 boundary. * ============================================================================ */ #define RSTENTRYID 0 #define RESETCTRLADDR 0xC3D00000 #define RESETCTRLSIZE 0x80 /** ============================================================================ * @name CODEMEMORYADDR/CODEMEMORYSIZE * * @desc Indicates startaddress/size for dsplink code region. * ============================================================================ */ #define CODEENTRYID 1 #define CODEMEMORYADDR (RESETCTRLADDR + RESETCTRLSIZE) #define CODEMEMORYSIZE 0x1FFF00u /** ============================================================================ * @name SHAREDENTRYID/SHAREDMEMORYADDR/SHAREDMEMORYSIZE * * @desc Indicates startaddress/size for dsplink shared memory region. * ============================================================================ */ #define SHAREDENTRYID0 2 #define SHAREDMEMORYADDR0 (CODEMEMORYADDR + CODEMEMORYSIZE) #define SHAREDMEMORYSIZE0 0x5000 /** ============================================================================ * @name SHAREDENTRYID/SHAREDMEMORYADDR/SHAREDMEMORYSIZE * * @desc Indicates startaddress/size for dsplink shared memory region. * ============================================================================ */ #define SHAREDENTRYID1 3 #define SHAREDMEMORYADDR1 (SHAREDMEMORYADDR0 + SHAREDMEMORYSIZE0) #define SHAREDMEMORYSIZE1 0x2B000 /** ============================================================================ * @name POOLMEMORYADDR/POOLMEMORYSIZE * * @desc Indicates startaddress/size for dsplink POOL memory region. * ============================================================================ */ #define POOLENTRYID 4 #define POOLMEMORYADDR (SHAREDMEMORYADDR1 + SHAREDMEMORYSIZE1) #define POOLMEMORYSIZE 0x000D0000u /** ============================================================================ * @name LINKCFG_memTable_00 * * @desc Memory table ID 0. * ============================================================================ */ STATIC LINKCFG_MemEntry LINKCFG_memTable_00 [] = { { RSTENTRYID, /* ENTRY : Entry number */ "RESETCTRL", /* NAME : Name of the memory region */ RESETCTRLADDR, /* ADDRPHYS : Physical address */ RESETCTRLADDR, /* ADDRDSPVIRT : DSP virtual address */ (Uint32) -1, /* ADDRGPPVIRT : GPP virtual address (if known) */ RESETCTRLSIZE, /* SIZE : Size of the memory region */ FALSE, /* SHARED : Shared access memory? */ FALSE, /* SYNCD : Synchornized? */ }, { CODEENTRYID, /* ENTRY : Entry number */ "DDR", /* NAME : Name of the memory region */ CODEMEMORYADDR, /* ADDRPHYS : Physical address */ CODEMEMORYADDR, /* ADDRDSPVIRT : DSP virtual address */ (Uint32) -1, /* ADDRGPPVIRT : GPP virtual address (if known) */ CODEMEMORYSIZE, /* SIZE : Size of the memory region */ FALSE, /* SHARED : Shared access memory? */ FALSE, /* SYNCD : Synchornized? */ }, { SHAREDENTRYID0, /* ENTRY : Entry number */ "DSPLINKMEM", /* NAME : Name of the memory region */ SHAREDMEMORYADDR0, /* ADDRPHYS : Physical address */ SHAREDMEMORYADDR0, /* ADDRDSPVIRT : DSP virtual address */ (Uint32) -1, /* ADDRGPPVIRT : GPP virtual address (if known) */ SHAREDMEMORYSIZE0, /* SIZE : Size of the memory region */ TRUE, /* SHARED : Shared access memory? */ FALSE, /* SYNCD : Synchornized? */ }, { SHAREDENTRYID1, /* ENTRY : Entry number */ "DSPLINKMEM1", /* NAME : Name of the memory region */ SHAREDMEMORYADDR1, /* ADDRPHYS : Physical address */ SHAREDMEMORYADDR1, /* ADDRDSPVIRT : DSP virtual address */ (Uint32) -1, /* ADDRGPPVIRT : GPP virtual address (if known) */ SHAREDMEMORYSIZE1, /* SIZE : Size of the memory region */ TRUE, /* SHARED : Shared access memory? */ FALSE, /* SYNCD : Synchornized? */ }, { POOLENTRYID, /* ENTRY : Entry number */ "POOLMEM", /* NAME : Name of the memory region */ POOLMEMORYADDR, /* ADDRPHYS : Physical address */ POOLMEMORYADDR, /* ADDRDSPVIRT : DSP virtual address */ (Uint32) -1, /* ADDRGPPVIRT : GPP virtual address (if known) */ POOLMEMORYSIZE, /* SIZE : Size of the memory region */ TRUE, /* SHARED : Shared access memory? Logically */ FALSE, /* SYNCD : Synchornized? */ }, { 5, /* ENTRY : Entry number */ "DSPIRAM", /* NAME : Name of the memory region */ 0x11800000, /* ADDRPHYS : Physical address */ 0x11800000, /* ADDRDSPVIRT : DSP virtual address */ (Uint32) -1, /* ADDRGPPVIRT : GPP virtual address (if known) */ 0x40000, /* SIZE : Size of the memory region */ FALSE, /* SHARED : Shared access memory? */ FALSE, /* SYNCD : Synchornized? */ }, { 6, /* ENTRY : Entry number */ "DSPL1DRAM", /* NAME : Name of the memory region */ 0x11F00000, /* ADDRPHYS : Physical address */ 0x11F00000, /* ADDRDSPVIRT : DSP virtual address */ (Uint32) -1, /* ADDRGPPVIRT : GPP virtual address (if known) */ 0x8000, /* SIZE : Size of the memory region */ FALSE, /* SHARED : Shared access memory? */ FALSE, /* SYNCD : Synchornized? */ }, } ; /** ============================================================================ * @name LINKCFG_memTables * * @desc Array of memory tables in the system. * ============================================================================ */ STATIC LINKCFG_MemEntry * LINKCFG_memTables [] = { LINKCFG_memTable_00 /* Memory Table 0 */ } ; /** ============================================================================ * @name LINKCFG_ipsTable_00 * * @desc IPS table ID 0. * ============================================================================ */ STATIC LINKCFG_Ips LINKCFG_ipsTable_00 [] = { { "IPS", /* NAME : Name of the Inter-Processor-Signaling component */ (Uint32) 32, /* NUMIPSEVENTS : Number of IPS events to be supported */ (Uint32) SHAREDENTRYID0, /* MEMENTRY : Memory entry ID (-1 if not needed) */ (Uint32) 28, /* GPPINTID : Interrupt no. to used by the IPS on GPP-side. (-1 if uni-directional to DSP) */ (Uint32) 5, /* DSPINTID : Interrupt no. to used by the IPS on DSP-side. (-1 if uni-directional to GPP) */ (Uint32) 4, /* DSPINTVECTORID : Interrupt vector no. to used by the IPS on DSP-side. (-1 if uni-directional to GPP) */ (Uint32) 50000000, /* ARGUMENT1 : Poll value for which IPS waits while sending event (-1 if infinite) */ 0 /* ARGUMENT2 : Second IPS-specific argument */ }, { "IPS", /* NAME : Name of the Inter-Processor-Signaling component */ (Uint32) 32, /* MAXIPSEVENTS : Number of IPS events to be supported */ (Uint32) SHAREDENTRYID1, /* MEMENTRY : Memory entry ID (-1 if not needed) */ (Uint32) 29, /* GPPINTID : Interrupt no. to used by the IPS on GPP-side. (-1 if uni-directional to DSP) */ (Uint32) 67, /* DSPINTID : Interrupt no. to used by the IPS on DSP-side. (-1 if uni-directional to GPP) */ (Uint32) 5, /* DSPINTVECTORID : Interrupt vector no. to used by the IPS on DSP-side. (-1 if uni-directional to GPP) */ (Uint32) 50000000, /* ARGUMENT1 : Poll value for which IPS waits while sending event (-1 if infinite) */ 0 /* ARGUMENT2 : Second IPS-specific argument */ } } ; /** ============================================================================ * @name LINKCFG_ipsTables * * @desc Array of IPS tables in the system. * ============================================================================ */ STATIC LINKCFG_Ips * LINKCFG_ipsTables [] = { LINKCFG_ipsTable_00 /* IPS Table 0 */ } ; /** ============================================================================ * @name LINKCFG_poolTable_00 * * @desc Pool table ID 0. * ============================================================================ */ STATIC LINKCFG_Pool LINKCFG_poolTable_00 [] = { { "SMAPOOL", /* NAME : Name of the pool */ (Uint32) SHAREDENTRYID1, /* MEMENTRY : Memory entry ID (-1 if not needed) */ (Uint32) POOLMEMORYSIZE, /* POOLSIZE : Size of the pool (-1 if not needed) */ (Uint32) -1, /* IPSID : ID of the IPS used */ (Uint32) -1, /* IPSEVENTNO : IPS Event number associated with POOL */ POOLENTRYID, /* POOLMEMENTRY : Pool memory region section ID */ 0x0, /* ARGUMENT1 : First Pool-specific argument */ 0x0 /* ARGUMENT2 : Second Pool-specific argument */ } } ; /** ============================================================================ * @name LINKCFG_poolTables * * @desc Array of Pool tables in the system. * ============================================================================ */ STATIC LINKCFG_Pool * LINKCFG_poolTables [] = { LINKCFG_poolTable_00 /* Pool Table 0 */ } ; /** ============================================================================ * @name LINKCFG_dataTable_00 * * @desc Data driver table ID 0. * ============================================================================ */ STATIC LINKCFG_DataDrv LINKCFG_dataTable_00 [] = { { "ZCPYDATA", /* NAME : Name of the data driver */ 0, /* BASECHANNELID : Base channel ID for the driver */ 16, /* NUMCHANNELS : Number of channels supported */ 16384, /* MAXBUFSIZE : Maximum size of buffer supported (-1 if no limit) */ (Uint32) SHAREDENTRYID1, /* MEMENTRY : Memory entry ID (-1 if not needed) */ 0, /* POOLID : Pool id for allocating buffers */ 1, /* QUEUELENGTH : Queue length for the data driver */ 1, /* IPSID : ID of the IPS used */ 1, /* IPSEVENTNO : IPS Event number associated with data Driver */ 0x0, /* ARGUMENT1 : First data driver specific argument */ 0x0 /* ARGUMENT2 : Second data driver specific argument */ } } ; /** ============================================================================ * @name LINKCFG_dataTables * * @desc Array of Data driver tables in the system. * ============================================================================ */ STATIC LINKCFG_DataDrv * LINKCFG_dataTables [] = { LINKCFG_dataTable_00 /* Data Table 0 */ } ; /** ============================================================================ * @name LINKCFG_mqtObjects * * @desc Array of Message Queue Transport objects in the system. * ============================================================================ */ STATIC LINKCFG_Mqt LINKCFG_mqtObjects [] = { { "ZCPYMQT", /* NAME : Name of the Message Queue Transport */ (Uint32) SHAREDENTRYID1, /* MEMENTRY : Memory entry ID (-1 if not needed) */ (Uint32) -1, /* MAXMSGSIZE : Maximum message size supported (-1 if no limit) */ 1, /* IPSID : ID of the IPS used */ 0, /* IPSEVENTNO : IPS Event number associated with MQT */ 0x0, /* ARGUMENT1 : First MQT-specific argument */ 0x0 /* ARGUMENT2 : Second MQT-specific argument */ } } ; /** ============================================================================ * @name LINKCFG_ringIoObjects * * @desc Array of RINGIO objects in the system. * ============================================================================ */ STATIC LINKCFG_RingIo LINKCFG_ringIoObjects [] = { { "RINGIOTABLE", /* NAME : Name of the RingIO Table */ SHAREDENTRYID0, /* MEMENTRY : Memory entry ID (-1 if not needed) */ 64, /* NUMENTRIES : Number of RingIO entries supported */ 0, /* IPSID : ID of the IPS used */ 0 /* IPSEVENTNO : IPS Event number associated with RingIO */ } } ; /** ============================================================================ * @name LINKCFG_mplistObjects * * @desc Array of MPLIST objects in the system. * ============================================================================ */ STATIC LINKCFG_MpList LINKCFG_mplistObjects [] = { { "MPLISTTABLE", /* NAME : Name of the MpList Table */ SHAREDENTRYID1, /* MEMENTRY : Memory entry ID (-1 if not needed) */ 64, /* NUMENTRIES : Number of MpList entries supported */ (Uint32) -1, /* IPSID : ID of the IPS used */ (Uint32) -1 /* IPSEVENTNO : IPS Event number associated with MpList */ } } ; /** ============================================================================ * @name LINKCFG_mpcsObjects * * @desc Array of MPCS objects in the system. * ============================================================================ */ STATIC LINKCFG_Mpcs LINKCFG_mpcsObjects [] = { { "MPCS", /* NAME : Name of the MPCS Table */ SHAREDENTRYID1, /* MEMENTRY : Memory entry ID (-1 if not needed) */ 256, /* NUMENTRIES : Number of MPCS entries supported */ (Uint32) -1, /* IPSID : ID of the IPS used */ (Uint32) -1 /* IPSEVENTNO : IPS Event number associated with MPCS */ } } ; /** ============================================================================ * @name LINKCFG_gppObject * * @desc Configuration object for the GPP. * ============================================================================ */ STATIC LINKCFG_Log LINKCFG_logObject = { FALSE, /* GDMSGQPUT : GPP->DSP MSG Transfer - MSGQ_put call */ FALSE, /* GDMSGQSENDINT : GPP->DSP MSG Transfer - GPP sends interrupt */ FALSE, /* GDMSGQISR : GPP->DSP MSG Transfer - DSP receives interrupt */ FALSE, /* GDMSGQQUE : GPP->DSP MSG Transfer - Message queued at DSP */ FALSE, /* DGMSGQPUT : DSP->GPP MSG Transfer - MSGQ_put call */ FALSE, /* DGMSGQSENDINT : DSP->GPP MSG Transfer - DSP sends interrupt */ FALSE, /* DGMSGQISR : DSP->GPP MSG Transfer - GPP receives interrupt */ FALSE, /* DGMSGQQUE : DSP->GPP MSG Transfer - Message queued at GPP */ FALSE, /* GDCHNLISSUESTART : GPP->DSP CHNL Transfer - Entering inside ISSUE call */ FALSE, /* GDCHNLISSUEQUE : GPP->DSP CHNL Transfer - ISSUE: Buffer is queued in internal structure on GPP */ FALSE, /* GDCHNLISSUECOMPL : GPP->DSP CHNL Transfer - ISSUE call completed */ FALSE, /* GDCHNLXFERSTART : GPP->DSP CHNL Transfer - Initiating a buffer transfer by GPP */ FALSE, /* GDCHNLXFERPROCESS : GPP->DSP CHNL Transfer - Actual transfer of buffer is going to take place */ FALSE, /* GDCHNLXFERCOMPL : GPP->DSP CHNL Transfer - Buffer transfer is complete */ FALSE, /* GDCHNLRECLSTART : GPP->DSP CHNL Transfer - Entering RECLAIM call */ FALSE, /* GDCHNLRECLPEND : GPP->DSP CHNL Transfer - RECLAIM: Wait on a semaphore */ FALSE, /* GDCHNLRECLPOST : GPP->DSP CHNL Transfer - RECLAIM: Posting the Semaphore */ FALSE, /* GDCHNLRECLCOMPL : GPP->DSP CHNL Transfer - RECLAIM call completed */ FALSE, /* DGCHNLISSUEQUE : DSP->GPP CHNL Transfer - ISSUE: Buffer is queued in internal structure on DSP */ FALSE, /* DGCHNLXFERSTART : DSP->GPP CHNL Transfer - Initiating a buffer transfer by DSP */ FALSE, /* DGCHNLXFERPROCESS : DSP->GPP CHNL Transfer - Actual transfer of buffer is going to take place */ FALSE, /* DGCHNLXFERCOMPL : DSP->GPP CHNL Transfer - Buffer transfer is complete */ FALSE, /* DGCHNLRECLPEND : DSP->GPP CHNL Transfer - RECLAIM: Wait on a semaphore */ FALSE, /* DGCHNLRECLPOST : DSP->GPP CHNL Transfer - RECLAIM: Posting the Semaphore */ 10, /* MSGIDRANGESTART : MSG ID range: lower limit */ 20 /* MSGIDRANGEEND : MSG ID range: upper limit */ } ; /** ============================================================================ * @name LINKCFG_linkDrvObjects * * @desc Array of Link driver objects in the system. * ============================================================================ */ STATIC LINKCFG_LinkDrv LINKCFG_linkDrvObjects [] = { { "SHMDRV", /* NAME : Name of the link driver */ DRVHANDSHAKEPOLLCOUNT, /* HSHKPOLLCOUNT : Poll value for which handshake waits (-1 if infinite) */ (Uint32) SHAREDENTRYID1, /* MEMENTRY : Memory entry ID (-1 if not needed) */ 0, /* IPSTABLEID : ID of the IPS table used */ sizeof (LINKCFG_ipsTable_00) / sizeof (LINKCFG_Ips), /* IPSENTRIES : Number of IPS supported */ 0, /* POOLTABLEID : ID of the POOL table */ sizeof (LINKCFG_poolTable_00) / sizeof (LINKCFG_Pool), /* NUMPOOLS : Number of POOLs supported */ 0, /* DATATABLEID : ID of the data driver table */ sizeof (LINKCFG_dataTable_00) / sizeof (LINKCFG_DataDrv), /* NUMDATADRV : Number of data drivers supported */ 0, /* MQTID : ID of the MQT */ 0, /* RINGIOTABLEID : RingIO Table Id used for this DSP */ 0, /* MPLISTTABLEID : MpList Table Id used for this DSP */ 0 /* MPCSTABLEID : MPCS Table ID used for this DSP */ }, } ; /** ============================================================================ * @name LINKCFG_dspObjects * * @desc Array of configuration objects for the DSPs in the system. * ============================================================================ */ STATIC LINKCFG_Dsp LINKCFG_dspObject = { "DA8XXGEM", /* NAME : Name of the DSP */ DspArch_C64x, /* ARCHITECTURE : DSP architecture */ "COFF", /* LOADERNAME : Name of the DSP executable loader */ FALSE, /* AUTOSTART : Autostart the DSP (Not supported) */ "DEFAULT.OUT", /* EXECUTABLE : Executable for autostart */ DSP_BootMode_Boot_Pwr, /* DOPOWERCTRL : Link does the Power Ctrl of DSP. */ RESETCTRLADDR, /* RESUMEADDR : Resume address */ RESETCTRLADDR, /* RESETVECTOR : Reset Vector for the DSP */ RESETCTRLSIZE, /* RESETCODESIZE : Size of code at DSP Reset Vector */ 1, /* MADUSIZE : DSP Minimum Addressable Data Unit */ (Uint32) -1, /* CPUFREQ : DSP Frequency (in KHz), -1 if default setting is to be used */ Endianism_Little, /* ENDIAN : DSP Endianism */ FALSE, /* WORDSWAP : Words must be swapped when writing to memory */ 0, /* MEMTABLEID : ID of the memory table used */ sizeof (LINKCFG_memTable_00)/sizeof (LINKCFG_MemEntry), /* MEMENTRIES : Number of entries in memory table */ 0, /* LINKDRVID : ID of the link driver used */ 0, /* ARG1 : Bus No of PCI card */ 0, /* ARG2 : Slot No of PCI card */ 0, /* ARG3 : DSPLINK Shared memory region for control data structures creation */ 0, /* ARG4 : Unused */ 0 /* ARG5 : Unused */ } ; /** ============================================================================ * @name DA8XXGEM_SHMEM_Config * * @desc DSP/BIOS LINK configuration structure. * ============================================================================ */ LINKCFG_DspConfig DA8XXGEM_SHMEM_Config = { (LINKCFG_Dsp *) &LINKCFG_dspObject, /* DSPOBJECTS : Array of DSP objects */ sizeof (LINKCFG_linkDrvObjects)/sizeof (LINKCFG_LinkDrv), /* NUMLINKDRVS : Number of Link Drviers*/ (LINKCFG_LinkDrv *) LINKCFG_linkDrvObjects, /* LINKDRVOBJECTS : Array of Link Driver objects */ sizeof (LINKCFG_memTables)/sizeof (LINKCFG_MemEntry *), /* NUMMEMTABLES : Number of memory tables */ (LINKCFG_MemEntry **) LINKCFG_memTables, /* MEMTABLES : Array of Memory tables */ sizeof (LINKCFG_ipsTables)/sizeof (LINKCFG_Ips *), /* NUMIPSTABLES : Number of IPS tables */ (LINKCFG_Ips **) LINKCFG_ipsTables, /* IPSTABLES : Array of IPS tables */ sizeof (LINKCFG_poolTables)/sizeof (LINKCFG_Pool *), /* NUMPOOLTABLES : Number of POOL tables */ (LINKCFG_Pool **) LINKCFG_poolTables, /* POOLTABLES : Array of Pool tables */ sizeof (LINKCFG_dataTables)/sizeof (LINKCFG_DataDrv *), /* NUMDATATABLES : Number of data tables */ (LINKCFG_DataDrv **) LINKCFG_dataTables, /* DATATABLES : Array of data tables */ sizeof (LINKCFG_mqtObjects)/sizeof (LINKCFG_Mqt), /* NUMMQTS : Number of MQTs */ (LINKCFG_Mqt *) LINKCFG_mqtObjects, /* MQTOBJECTS : Array of MQT objects */ sizeof (LINKCFG_ringIoObjects)/sizeof (LINKCFG_RingIo), /* NUMRINGIOTABLES: Number of RINGIO tables */ (LINKCFG_RingIo *) LINKCFG_ringIoObjects, /* RINGIOOBJECTS : Array of RINGIO objects */ sizeof (LINKCFG_mplistObjects)/sizeof (LINKCFG_MpList), /* NUMMPLISTTABLES: Number of MPLIST tables */ (LINKCFG_MpList *) LINKCFG_mplistObjects, /* MPLISTOBJECTS : Array of MPLIST objects */ sizeof (LINKCFG_mpcsObjects)/sizeof (LINKCFG_Mpcs), /* NUMMPCSTABLES : Number of MPCS tables */ (LINKCFG_Mpcs *) LINKCFG_mpcsObjects, /* MPCSOBJECTS : Array of MPCS objects */ (LINKCFG_Log *) &LINKCFG_logObject, /* LOGOBJECT : Pointer to LOG object */ } ; #if defined (__cplusplus) } #endif /* defined (__cplusplus) */
/** ============================================================================ * @file dsplink-omapl138gem-base.tci * * @path $(DSPLINK)/dsp/inc/DspBios/5.XX/OMAPL138GEM/ * * @desc This file defines base configuration for DSP/BIOS LINK. * * @ver 1.65.01.05_eng * ============================================================================ * Copyright (C) 2002-2009, Texas Instruments Incorporated - * http://www.ti.com/ * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ============================================================================ */ /* ============================================================================ * Load assert support * ============================================================================ */ utils.importFile("assert.tci"); /* ============================================================================ * Load base TCI file. * ============================================================================ */ utils.loadPlatform("ti.platforms.evmOMAPL138") ; /* ============================================================================ * Enable common BIOS features used by all examples * ============================================================================ */ bios.disableRealTimeAnalysis(prog); bios.enableMemoryHeaps(prog); bios.disableRtdx(prog); bios.enableTskManager(prog); /* ============================================================================ * GBL * ============================================================================ */ prog.module("GBL").ENABLEALLTRC = false ; prog.module("GBL").PROCID = parseInt (arguments [0]) ; prog.module("GBL").C64PLUSCONFIGURE = true ; prog.module("GBL").C64PLUSL2CFG = "32k" ; prog.module("GBL").C64PLUSL1DCFG = "32k" ; prog.module("GBL").C64PLUSMAR192to223 = 0x00000008 ; /* ============================================================================ * MEM * ============================================================================ */ prog.module("MEM").STACKSIZE = 0x1000 ; /* ============================================================================ * MEM : RESET_VECTOR * ============================================================================ */ var RESET_VECTOR = prog.module("MEM").create("RESET_VECTOR"); RESET_VECTOR.base = 0xC3D00000 ; RESET_VECTOR.len = 0x00000080; RESET_VECTOR.space = "code/data"; RESET_VECTOR.createHeap = false; RESET_VECTOR.comment = "RESET_VECTOR"; /* ============================================================================ * MEM : DDR * ============================================================================ */ var DDR = prog.module("MEM").instance("DDR"); DDR.base = RESET_VECTOR.base + RESET_VECTOR.len ; DDR.len = 0x1FFF00; DDR.space = "code/data"; DDR.createHeap = true; DDR.heapSize = 0x10000; DDR.comment = "DDR"; /* ============================================================================ * MEM : DSPLINKMEM * ============================================================================ */ var DSPLINKMEM = prog.module("MEM").create("DSPLINKMEM"); DSPLINKMEM.base = DDR.base + DDR.len; DSPLINKMEM.len = 0x30000; DSPLINKMEM.createHeap = false; DSPLINKMEM.comment = "DSPLINKMEM"; /* ============================================================================ * MEM : POOLMEM * ============================================================================ */ var POOLMEM = prog.module("MEM").create("POOLMEM"); POOLMEM.base = DSPLINKMEM.base + DSPLINKMEM.len ; POOLMEM.len = 0xD0000 ; POOLMEM.createHeap = false; POOLMEM.comment = "POOLMEM"; /* ============================================================================ * MEM : IRAM * ============================================================================ */ var IRAM = prog.module("MEM").instance("IRAM"); IRAM.base = 0x11800000 ; IRAM.len = 0x8000 ;
Please help me to solve this problem.
Thanks in advance.