hi all
I am using DVRRDK_02.00.00.23
when running the demo including SCD-motion algorithm
how can i set so as to get warming message result from detecting motion in camera
thank you for any help
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi all
I am using DVRRDK_02.00.00.23
when running the demo including SCD-motion algorithm
how can i set so as to get warming message result from detecting motion in camera
thank you for any help
Which usecase you are running?
By default tamper and motion detection mode is enabled in some of the usecases. For tamper you should get tamper detection message if you unplug the input source or block the camera lense.
For motion detection by default all the blocks are disabled for monitoring. For motion detection you need to enable block no.s that you want to monitor. Please refer section 2.1.2 in demoguide doc "DM81xx_DVR_RDK_DemoGuide.pdf" for more details on how to activate particular block.